SSZTDB0 September 2025 LM5180-Q1 , LMG3522R030-Q1 , SN6507-Q1 , UCC14341-Q1 , UCC25800-Q1
Small, isolated power supplies provide power across isolation barriers in applications from electric vehicle traction inverters to factory control modules. In this Power Tip, I’ll examine different isolated bias-supply topologies and their electromagnetic interference (EMI) performance. As you’ll see, parasitic capacitance across the isolation transformer is a major contributor to common-mode noise propagation.
In traction inverters, gate drivers actuate the high-power switches—usually insulated-gate bipolar transistors (IGBTs) or silicon carbide (SiC) MOSFETs—which convert energy between the high-voltage battery and the electric machine (see Figure 1). The gate drivers are typically isolated, with one part of the gate driver IC connected to the low-voltage domain (the primary side) and another part connected to the high-voltage domain (the secondary side). The gate-drive control signals come from a microcontroller on the primary side and are passed through to the secondary side to turn the power switch on and off.
Figure 1 A traction inverter with
isolated gate drivers. Source: Texas Instruments
The secondary side of the isolated gate driver needs an isolated power supply in order to actuate power switch turn-on and turn-off (see Figure 2).
Figure 2 An isolated bias supply
provides power across the isolation barrier for the isolated gate driver.
Source: Texas InstrumentsThe power ratings for isolated bias supplies are usually fairly low—less than 10 W. The equation below estimates their power requirements as:
where VDRV is the gate-drive voltage, Qg is the switch gate charge, and FSW is the switching frequency of the switch (not the isolated bias-supply switching frequency). The gate-drive voltage depends on which switch you select, but typically ranges from +15V to +25V on the positive rail and –8V to 0V on the negative rail.
Common topologies for isolated bias supplies include flyback, push-pull and inductor-inductor-capacitor (LLC). Some fully integrated power modules (that include the transformer in the package) use a full-bridge configuration on the primary side. Flyback converters, such as the LM5180-Q1 from Texas Instruments (TI), are well known, provide good output voltage regulation, are fairly efficient, can be designed without an optocoupler (using primary-side regulation), and can have multiple isolated outputs. Their drawbacks are that they tend to be limited in frequency range (<350kHz) and have a large transformer size. Push-pull converters, such as TI’s SN6507-Q1 and LLC converters, such as TI’s UCC25800-Q1, are simple but do not have closed-loop feedback. As a result, the output voltage regulation suffers, potentially requiring a pre-regulator, a post-regulator, or both. Integrated power modules (such as TI’s UCC14341-Q1) can regulate the output voltage and are simple and small, but their drawbacks are limited power output (typically <1.5W) and lower efficiency than alternative options.
One question you may have is about the EMI performance of different topologies: Do certain topologies have more or less impact on electromagnetic compatibility results? To address these questions, let’s first examine the isolation transformer. Some parasitic capacitance does exist between the windings of the transformer, which charges or discharges when the traction inverter switch node (VSW) switches between HV+ and HV– nodes. A short pulse of common-mode current charges or discharges the parasitic capacitance during the switching transition. The common-mode current is directly proportional to the parasitic capacitance and the switch-node slew rate (dv/dt). Large capacitance or faster switch-node slew rates—as you might see with wide band-gap semiconductors such as gallium nitride (GaN) and SiC—will result in more common-mode current. Figure 3 highlights this parasitic capacitance and the common-mode current used to charge and discharge it.
Figure 3 Common-mode current charges
the transformer parasitic capacitance when the switch node (VSW)
transitions. Source: Texas InstrumentsConverter topology does influence transformer design and the resulting parasitic capacitance. Flyback converter transformers (or coupled inductors if you prefer that nomenclature) are designed to have strong coupling between the primary and secondary sides in an effort to reduce leakage inductance. Leakage inductance causes unwanted voltage spikes and power loss in snubber circuits. The unfortunate impact of designing for low leakage inductance is that the interwinding capacitance typically increases, and can be 20pF or more. On the other hand, it is possible to design LLC converters to use a transformer’s leakage inductance in its resonant tank. As a result, you would not need to design the transformers to minimize leakage inductance; they can have a parasitic capacitance around 2pF. As you’ll see, this helps reduce common-mode currents.
Table 1 shows some parameters from a study of four isolated bias topologies to experimentally validate the impact of transformer parasitic capacitance on common-mode current. All of the converters were designed for a 15VIN, 15VOUT, 1.5W application. The switching frequency of each topology is based on typical values, with the transformers designed accordingly. As you can see, the flyback converter transformer has the lowest leakage inductance and the highest parasitic capacitance. The LLC converter transformer has the highest leakage inductance and the lowest parasitic capacitance.
|
Comparing these isolated bias-supply topologies involved performing an extensive set of tests: efficiency, load regulation, input and output ripple, thermals, and conducted and radiated EMI. To focus on the common-mode current measured between the isolated grounds in the system, my colleagues connected a wire between the two grounds and measured the common-mode current when the high-power switches (in this example, a GaN half bridge using the LMG3522R030-Q1) turned on and off at 400V. Figure 4 and Figure 5 show the results for a high-voltage switch-node slew rate of 40V/ns and 100V/ns, respectively.
Figure 4 Common-mode current comparison
at a 40V/ns slew rate on the switch node. Channel 1 is the high-voltage switch
node (200V/div) and Channel 2 is the common-mode current (500mA/div). Source:
Texas Instruments
Figure 5 Common-mode current comparison
at a 100V/ns slew rate on the switch node. Channel 1 is the high-voltage switch
node (200V/div) and Channel 2 is the common-mode current (500mA/div). Source:
Texas InstrumentsThe measured results demonstrate that the common-mode current for the flyback transformer was the largest (935mA and 1,420mA for 40V/ns and 100V/ns slew rates). This is to be expected, since the transformer had the largest parasitic capacitance. And because the LLC converter had the lowest parasitic capacitance, the common-mode current measured was the smallest (197mA and 570mA for 40V/ns and 100V/ns slew rates). Large common-mode current spikes are detrimental, since they can conduct noise from the high-voltage domain to the low-voltage domain, cause ground bounce; and potentially lead to poor converter operation including skipped pulses, lost regulation, or unexpected shutdowns.
Common-mode currents can be especially difficult to mitigate. One of the best ways to address common-mode current issues is to avoid generating common-mode current in the first place. While the application discussed here was a traction inverter in an electric vehicle, the principles apply to applications such as grid-connected converters and server power supplies.
Previously published on EDN.com.