SWCU185F january 2018 – march 2023 CC1312R , CC1352P , CC1352R , CC2642R , CC2642R-Q1 , CC2652P , CC2652PSIP , CC2652R , CC2652RB , CC2652RSIP , CC2662R-Q1
Command ID number: 0x0402
CMD_STOP is a direct command.
On reception, the radio CPU informs the radio operation command currently running that it is requested to stop. The CMD_STOP command is more graceful than the CMD_ABORT command, but might take more time to finish. Normally, a packet being received or transmitted is handled to completion. The exact behavior on reception of CMD_STOP is described for each radio operation command. Some commands always end in a known time and do not respond to CMD_STOP.
If no radio operation command is running, no action is taken. The result signaled in CMDSTA is done in all cases. If a radio operation command is running, CMDSTA may be updated before the radio operation ends.