SWCU185F january 2018 – march 2023 CC1312R , CC1352P , CC1352R , CC2642R , CC2642R-Q1 , CC2652P , CC2652PSIP , CC2652R , CC2652RB , CC2652RSIP , CC2662R-Q1
There are two main event fabric blocks in the CC13x2 and CC26x2 devices. One in the MCU power domain (MCU event fabric) and the other in the AON power domain (AON event fabric). Figure 6-4 shows a simplified overview of the two modules together. The MCU event fabric is one of the subscribers to the AON event fabric.