SWCU185F january 2018 – march 2023 CC1312R , CC1352P , CC1352R , CC2642R , CC2642R-Q1 , CC2652P , CC2652PSIP , CC2652R , CC2652RB , CC2652RSIP , CC2662R-Q1
The CMD_PROP_RESTART_RX command is a direct command that takes no parameters.
CMD_PROP_RESTART_RX must only be sent while a CMD_PROP_RX or CMD_PROP_RX_ADV command is running. If a packet is being received, reception is aborted as described in Section 26.10.5.4 and the packet returns to sync search.
If the command is issued without an RX command running, the radio CPU returns the result ContextError in CMDSTA. Otherwise, the radio CPU returns DONE.