SWCU185F january 2018 – march 2023 CC1312R , CC1352P , CC1352R , CC2642R , CC2642R-Q1 , CC2652P , CC2652PSIP , CC2652R , CC2652RB , CC2652RSIP , CC2662R-Q1
Auto mode is similar to basic mode, except that when a transfer request is received, the transfer completes, even if the μDMA request is removed. This mode is suitable for software-triggered transfers. Generally, auto mode is not used with a peripheral.
The μDMA controller sets the mode for that channel to stop when all the items have been transferred using auto mode.