SWCU185F january 2018 – march 2023 CC1312R , CC1352P , CC1352R , CC2642R , CC2642R-Q1 , CC2652P , CC2652PSIP , CC2652R , CC2652RB , CC2652RSIP , CC2662R-Q1
Sample words are stored to memory in little-endian byte order, meaning that the least significant byte (LSByte) is stored at the lower byte address, and the most significant byte (MSByte) is stored at the higher byte address.
If both ADx pins are configured as input or both ADx pins are configured as output, the sample words for each audio channel are stored AD0 first and AD1 last.
Figure 25-6, Figure 25-7, Figure 25-8, Figure 25-9, and Figure 25-10 show examples of sample storage for typical use cases (F = frame index, C = channel index, P = ADx pin index).