SWCU185F january 2018 – march 2023 CC1312R , CC1352P , CC1352R , CC2642R , CC2642R-Q1 , CC2652P , CC2652PSIP , CC2652R , CC2652RB , CC2652RSIP , CC2662R-Q1
The ADC connects to a FIFO that can hold up to
four ADC samples. Read AUX_ANAIF:ADCFIFO to get
the oldest sample. It is possible to write dummy
samples to the FIFO for debug purposes. The FIFO
samples are not compensated for offset and gain
errors in the ADC. The user must perform the
compensation manually using the factory
configuration data stored during chip production,
see
Section 12.2.1. The System CPU can use the AUX_ADC
TI-DriverLib module to accomplish this task.
AUX_ANAIF:ADCFIFOSTAT provides FIFO status flags such as overflow, underflow, and utilization. All FIFO status flags and the ADC-conversion-done event connect to the AUX event bus.
To recover from an overflow or underflow condition, the user must flush the FIFO and re-enable the digital ADC interface, as described in AUX_ANAIF:ADCCTL.CMD (see Section 20.8.8).
When debugging the software, showing the AUX_ANAIF_ADCFIFO register causes JTAG to read the FIFO, which pops the sample from the FIFO, and consequently the software cannot read it.