SWCU185F january 2018 – march 2023 CC1312R , CC1352P , CC1352R , CC2642R , CC2642R-Q1 , CC2652P , CC2652PSIP , CC2652R , CC2652RB , CC2652RSIP , CC2662R-Q1
This manual makes frequent use of certain terms. These terms refer to structures that the crypto core uses for operations.
External memory: A memory that is externally attached to the crypto core AHB master port, and only accessible using DMAC operations
Slave interface (host processor bus): Interface of the crypto core that the host processor uses to read or write registers of the engine
Tag or digest: Two interchangeable terms that indicate the result of an authentication operation. The term digest is used for regular hash operations, while tag is used for authenticated encryption operations (AES-CCM).
Crypto context: A collection of parameters that define the crypto operation: mode, key, IV, and so forth