SWCU194 March 2023 CC1314R10 , CC1354P10 , CC1354R10 , CC2674P10 , CC2674R10
Command ID number: 0x040A
CMD_DISARM_RAT_CH is an immediate command that takes the parameters listed in Table 26-47.
| Byte Index | Field Name | Bits | Bit Field Name | Type | Description |
|---|---|---|---|---|---|
| 0–1 | commandNo | W | The command ID number | ||
| 2 | ratCh | W | The RAT channel number |
On reception, the radio CPU disarms the RAT channel given by ratCh.
CMD_DISABLE_RAT_CH may be sent as a direct command. If so, ratCh is given by the parameter in bits 8–15 of CMDR.
The channel number must indicate a channel not reserved for use by the radio CPU. Otherwise, the radio CPU returns ParError in RFC_DBELL:CMDSTA. If the channel number is valid, the CPU returns Done in CMDSTA after the channel is armed.