SWRA466D February 2015 – August 2021 CC1310 , CC1310 , CC1352R , CC1352R , CC2538 , CC2538 , CC2620 , CC2620 , CC2630 , CC2630 , CC2640 , CC2640 , CC2640R2F , CC2640R2F , CC2640R2F-Q1 , CC2640R2F-Q1 , CC2642R , CC2642R , CC2642R-Q1 , CC2642R-Q1 , CC2650 , CC2650 , CC2650MODA , CC2650MODA , CC2652R , CC2652R , CC2652R7 , CC2652R7 , CC2652RB , CC2652RB , CC2652RSIP , CC2652RSIP
The example application for SBL is created for Visual Studio C++ Professional 2015 and is tested using the hardware included in the CC2538, CC2650, and CC2652R development kits and. The example application can be downloaded in the following URL: http://www.ti.com/lit/zip/swra466
SblAppEx is a test application that performs the following actions using the CC2538, CC26x0, or CC26x2 ROM bootloader:
A successful execution of the test application should look similar to Figure 4-1.