SWRA495L December 2015 – April 2025 CC1310 , CC1350 , CC2620 , CC2630 , CC2640 , CC2640R2F , CC2640R2F-Q1 , CC2642R-Q1 , CC2650 , CC2662R-Q1
TI intends the amplitude control loop to regulate the amplitude of the oscillations of the crystal for best performance. The following are the two primary portions of the control loop:
To turn on the crystal so that the radio can operate, start-up is required. Steady state amplitude regulation is not required for the crystal or radio to function.