SWRU580 April 2021 CC2564C , CC2564MODA , CC2564MODN
The Find Me profile defines the behavior when a button is pressed on a device to cause an immediate alert on a peer device. This can be used to allow users to find devices that have been misplaced. There are two roles defined in this profile, Server and the Client.
This application allows the user to use a console to use Bluetooth Low Energy (BLE) to establish connection between two BLE devices, change phone alert status, change ringer status, put in and get out of silent mode.
It is recommended that the user visits the kit setup Getting Started Guide for MSP430, Getting Started Guide for MSP432 or Getting Started Guide for STM32F4 pages before trying the application described on this page.
Running the Bluetooth CodeOnce the code is flashed, connect the board to a PC using a miniUSB or microUSB cable. Once connected, wait for the driver to install. It will show up as MSP-EXP430F5438 USB - Serial Port (COM x), XDS110 Class Application/User UART (COM x) for MSP432, under Ports (COM & LPT) in the Device manager. Attach a Terminal program like PuTTY to the serial port x for the board. The serial parameters to use are 115200 Baud (9600 for MSP430), 8, n, 1. Once connected, reset the device using Reset S3 button (located next to the mini USB connector for the MSP430) and you should see the stack getting initialized on the terminal and the help screen will be displayed, which shows all of the commands.
Figure 20-1 FMP Demo Start