SWRU616B September 2023 – April 2024 CC3300 , CC3300MOD , CC3301 , CC3301MOD , CC3350 , CC3350MOD , CC3351 , CC3351MOD
A PIN method is another option for establishing the WPS connection. In this case, one Wi-Fi device has a pre-defined PIN key printed on the label, usually 8 digits in length, while the other Wi-Fi device inserts this key after starting the WPS connection process. The side with the pre-defined key is called Label and the device inserting the key is called Keypad. Both relate to the PIN method. After inserting the key, the connection process is the same as with the PBC method.