The LP-EM-CC2745R10-Q1 has two user-configurable jumpers, as shown in Figure 2-1:
- When the P2 LaunchPad jumper is connected across pins 1 and 2, this will connect DIO16 to the onboard Red LED. When removed, the jumper allows direct connection of DIO16 to the BoosterPack header J2:36.
- When the P2 LaunchPad jumper is connected across pins 3 and 4, this will connect DIO12 to the onboard Green LED. When removed, the jumper allows direct connection of DIO12 to the BoosterPack header J2:19.
In addition the LP-EM-CC2745R10-Q1 has 2 additional jumpers that allow access to both 5V and GND via header P5 and 3.3V and GND through header P1, as shown in Figure 2-1.