SWRZ121B February   2022  – October 2026 CC2651R3

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Advisories Matrix
  5. 2Nomenclature, Package Symbolization, and Revision Identification
    1. 2.1 Device and Development Support-Tool Nomenclature
    2. 2.2 Devices Supported
    3. 2.3 Package Symbolization and Revision Identification
  6. 3Advisories
    1.     Radio_04
    2.     Power_03
    3.     I2C_01
    4.     I2S_01
    5.     CPU_01
    6.     CPU_02
    7.     CPU_Sys_01
    8.     Sys_01
    9.     Sys_05
    10.     SYSCTRL_01
    11.     ADC_01
    12.     ADC_02
    13.     ADC_03
  7. 4Revision History

ADC_01

Periodic ADC trigger at 200 kHz rate can be ignored when XOSC_HF is turned on or off

Revisions Affected:

Revision C and earlier

Details:

There is no dedicated clock source selection for the ADC clock. The clock is derived from either XOSC_HF or RCOSC_HF, but defaults to XOSC_HF-derived clock whenever this is turned on.

When the ADC clock source is switched from RCOSC_HF to XOSC_HF-derived clock, the clock will stop for 2 cycles (24 MHz).

When the ADC clock source is switched from XOSC_HF-derived clock to RCOSC_HF-derived clock, the clock will stop for additionally 12 clock cycles, as the RCOSC_HF-derived clock is not ready when switch is done.

The fact that the clock is stopped, together with the difference in frequency between XOSC_HF and RCOSC_HF, may cause the ADC sampling and conversion to finish too late to catch the next trigger.

Workaround 1:

Use asynchronous sampling.

The sampling period after the issue occurs can be reduced by up to 20% (12 + 1 clock cycles at 24 MHz)

To use the ADC in asynchronous mode, by using the ADCBuf driver:

ADCBuf_Params params;
ADCBufCC26X2_ParamsExtension paramsExtension;

ADCBuf_Params_init(&params);
ADCBufCC26X2_ParamsExtension_init(&paramsExtension);

paramsExtension.samplingMode = ADCBufCC26X2_SAMPING_MODE_ASYNCHRONOUS;
params.custom = &paramsExtension;

To use the ADC in asynchronous mode, by using DriverLib API:

Call AUXADCEnableAsync()to enable the ADC, instead of AUXADCEnableSync()

Example:

AUXADCEnableAsync(AUXADC_REF_FIXED, AUXADC_TRIGGER_GPT0A);

Please note the difference between the asynchronous and synchronous ADC modes:

  • In asynchronous mode, the ADC trigger ends the sampling period (which started immediately after the previous conversion), and starts conversion.
  • In synchronous mode, the ADC trigger starts the sampling period (with configurable duration), followed by conversion.

Workaround 2:

Ensure that XOSC_HF is not turned on or off while the ADC is used.

Workaround 3:

Increase the sampling period by (12+1)/24 µs or more.