TIDUCJ0G November   2016  – April 2020

 

  1.   Revision History

Base Board Settings

The design follows a HSEC control card concept. Any device for which a HSEC control card is available from the C2000 MCU product family can be potentially used on this design. The key resources used for controlling the power stage on the MCU are listed in Table 2. Figure 15 shows the key power stage and connectors on the design guide, and Table 3 lists the key connectors and their functions. To get started:

  1. Make sure no power source is connected to the design.
  2. Insert the control card in the J8-J10 slot.
  3. Insert a jumper at J11 and J12 to connect the bias supply for 5 V and 3.3 V .
  4. Connect a 12-V DC, 1-Amps power supply at J4. A few LEDs on the base board will light up indicating power. The LED on the control card will also light up. This light indicates the device is powered up as well.
  5. NOTE

    The bias for the MCU is separated from the power stage, which enables safe bring up of the system.

  6. To connect JTAG, use a USB cable from the control card and connect it into a host computer.
  7. A three-phase power supply is connected to the input J2. The board works as a three-wire system, therefore, the connection of the neutral is not required. A virtual neutral is generated on the board for sensing purpose of VL-N voltages.
  8. A resistive load of approximately 500Ω should also be connected to the output at J1. The load is connected across the positive and negative terminal (Vbus). The midpoint (M) is not connected to the load.
  9. Current and voltage probes can be connected to observe the input current, input voltage, and output voltages, as shown in Figure 16.
Figure 15. Board OverviewTIDM-1000 Board_Annotated.gif

Table 2. Key Controller Peripherals Used for Control of Power Stage on Board

SIGNAL NAME HSEC PIN NUMBER FUNCTION
PWM-1A 49 PWM: Vienna rectifier PWM Ph1A
PWM-1B 51 PWM: Vienna rectifier PWM Ph1B
PWM-2A 53 PWM: Vienna rectifier PWM Ph2A
PWM-2B 55 PWM: Vienna rectifier PWM Ph2B
PWM-3A 50 PWM: Vienna rectifier PWM Ph3A
PWM-3B 52 PWM: Vienna rectifier PWM Ph3B
IL1 15, 20 ADC with CMPSS: Inductor current measurement Ph1
IL2 21.27 ADC with CMPSS: Inductor current measurement Ph2
IL3 25 ADC with CMPSS: Inductor current measurement Ph3
V1 18 ADC: AC voltage sensing Ph1
V2 28 ADC: AC voltage sensing Ph2
V3 34 ADC: AC voltage sensing Ph3
Vbus_PM 31, 24 ADC: Bus voltage positive terminal to midpoint
Vbus_MN 37, 26 ADC: Bus voltage midpoint to negative terminal
Profiling GPIO1 58 GPIO: Used to profile code (optional)
Profiling GPIO2 60 GPIO: Used to profile code (optional)

Table 3. Key Connectors and Function

CONNECTOR NAME FUNCTION
J1 Output high voltage bus
J2 Input three phase voltage
J3 Neutral and Earth connection
J4 Input bias supply, 12-V DC 1 Amps
J5 DAC output for debugging
J6 Ground
J7 Profiling GPIO connector
J8,J10 HSEC control card connector slot
J9 Remote enable connector
J11 5-V jumper, used to disconnect the 5-V supply
J12 3-V jumper, used to disconnect the 12-V jumper
Figure 16. Hardware Setup to Run SoftwareTIDM-1000 HWSetupImage.gif