TIDUE71D March   2018  – April 2020

 

  1.   Revision History

Gating Parameters

The gating parameters set is used in the association process to provide a boundary for the points that can be associated with a given track. These parameters are target-specific. Table 9 lists each of these parameters.

Table 9. Gating Function Parameters

PARAMETER DEFAULT DIM DESCRIPTION
Gain 3 Gating gain
LengthLimit 1.5 m Gating limit in length
WidthLimit 1.5 m Gating limit in width
HeightLimit 2 m Gating limit in height
VelocityLimit 20 m/s Gating limit in velocity (0 – no limit)

The gating gain is a factor by which the gating volume can be increased to search for points to associate with the track. The gating volume can be estimated as the volume of the ellipsoid, computed as TIDEP-01000 section33315.png, where a, b, and c are the expected target dimensions in range (m), angle (rad), and doppler (m/s).

For example, consider a person as a radar target. For the target center, we could want to reach ±0.45 m in length (a = 0.9), ±3 degree in azimuth (b = 6π / 180), and ±5.18 m/s in radial velocity (c = 10.36), resulting in a volume of approximately 4.

In addition to setting the volume of the gating ellipsoid, the limits can be imposed to protect the ellipsoid from overstretching. The limits are the function of the geometry and motion of the expected targets. For example, setting the WidthLimit to 8 m does not allow the gating function to stretch beyond 8 m in width.