TIDUEB8C July 2018 – March 2021 TPS274160
The test case TCM_PHYL_INTF_IQPKHM tests the voltage drop on the high side of the IO-Link PHY during the wake-up pulse. Therefore the CQ line is loaded with 26 Ω and the wake-up pulse is generated. The voltage on the CQ line has to exceed 13 V to pass this test. This test is done with a L+ voltage of 20 V and 30 V.
Figure 3-8 Testcase TCM_PHYL_INTF_IQPKHM: Wake-Up Current High Side - 20 V L+ Resulting in 17.4 V
Figure 3-9 Testcase TCM_PHYL_INTF_IQPKHM: Wake-Up Current High Side - 30 V L+ Resulting in 26.4 VAs Figure 3-8 and Figure 3-9 show, the voltage is above 13 V, so the test of the high-side driver is passed.
The next relevant test case is TCM_PHYL_INTF_IQPKLM. This test is similar than before, but testing the low-side switch. Therefore the load is 24 Ω for 20 V L+ voltage and 44 Ω for 30 V. The resistor must be connected between L+ and CQ to test the low side. The voltage has to be below 8 V to pass this test.
Figure 3-10 Testcase TCM_PHYL_INTF_IQPKLM: Wake-Up Current Low Side - 20 V L+ Resulting in 2 V
Figure 3-11 Testcase TCM_PHYL_INTF_IQPKLM: Wake-Up Current Low Side - 30 V L+ Resulting in 2 VSo all the tests for the current capability during the wake-up pulse are passed.