TIDUEG2C March 2019 – March 2020
In this lab, the output current control loop is closed, with a resistive load connected on the secondary in parallel with a voltage source, to emulate a battery connection. Hardware is assumed to be set up as shown in Figure 52. Figure 53 shows the complete software diagram for this build.