TIDUEI1C November 2018 – April 2020
The MMWAVEICBOOST is an add-on board used with TI's mmWave sensor in all Starter Kits, to provide more interfaces and PC connectivity to the mmWave sensors. The MMWAVEICBOOST board provides an interface for the mmWave Studio tool to configure the radar device and capture the raw analog-to-digital converter (ADC) data using a capture board, such as the DCA1000 evaluation module (EVM). It also provides an interface to the MSP43xx boards through 40-pin LaunchPad™ / BoosterPack™ connectors.