TIDUET7G September 2019 – October 2023
, which launches a debugging session. In the case of dual CPU devices, a window may appear to select the CPU the debug must be performed. In this case, select CPU1. The project then loads on the device, and CCS debug view becomes active. The code halts at the start of the main routine.
) on the watch window to enable continuous update of values from the controller. The watch window appears as shown in Figure 3-11.
Figure 3-11 PFC Lab 2: Closed Current Loop Expressions View
button.
.
).