TIDUF20B December 2022 – July 2025
Use the following procedures before running this design board. The design was constructed with 32s pack configurations. The board was tested using DC source and 2700μF electrolytic capacitor in parallel to simulate the total pack. Twenty 200Ω resistors in series are used to divide the pack voltage and simulate 32s battery cells.
Figure 3-5 shows the charge process setup example.
Figure 3-6 shows the discharge process setup example using the following conditions.