TIDUF20B December 2022 – July 2025
The CAN interface can be used for communication between the BMU to stack the battery packs for high-cell-count systems, but address the CAN interface to a different ID because the default BMU CAN node ID is the same. Figure 2-8 shows the design using a hardwire wake-up CAN auto address.
BMUs are cascaded and waked up one by one. Every BMU has a wake input signal for waking and a wake output signal for waking the next BMU. The initial CAN node ID is defined by the host microcontroller. The BMU keeps monitoring the CAN frame for when to be waked up and uses the ID in data field as an ID, then sends ID+1 CAN frame to the CAN BUS and wake out signal through GPIO. Figure 2-9 shows a method where the wake signal pattern meets the timing for a more robust design.