The following steps are recommended to
test the communication between two Bluetooth devices:
- Set jumpers JP6 and JP7 to enable
the Bluetooth connection (position 1-2 for both).
- Connect a PC with the SmartRF Studio 8 application through a cable with
the USB Type-C connector.
- Start the SmartRF
Studio 8 application.
- Click on CC2340R5, which appears
in the XDS110 connection window.
- In the RX and TX tabs click
Start Test at the receiver first and then start the transmitter by
also clicking on Start Test.