TIDUF98A October 2024 – February 2025
To view the metrology parameter values from the GUI, perform the following steps:
Figure 2-7 GUI Configuration File Changed to Communicate With Energy Measurement
System
Figure 2-8 GUI Startup WindowWhen clicking the green button, the results window opens (see Figure 2-9). In the figure, there is a trailing "L" or "C" on the Power factor values to indicate an inductive or capacitive load, respectively. Note that by default, the column in the GUI labeled "Phase A" is actually the shunt channel and the column labeled "Neutral" is actually the CT channel. If the system and shunt is referenced with respect to the neutral, the shunt can actually measure the neutral current and the CT can measure the line current, unlike how the GUI is labeled.
Figure 2-9 GUI
Results WindowFrom the results window, the total-energy consumption readings can be viewed by clicking the Meter Consumption button. After the user clicks this button, the Meter events and consumption window pops up, as Figure 2-10 shows.
Figure 2-10 Meter
Events and Consumption WindowFrom the results window, the meter settings can be viewed by clicking the Meter features button, view the system calibration factors by clicking the Meter calibration factors button, or open the window used for calibrating the system by clicking the Manual cal. button.