TI (テキサス インスツルメンツ) は、強力なグローバル生産拠点を構えており、あらゆる環境において地政学的に信頼できる能力でお客様をサポートすることができます。
複数の拠点から技術や製品を調達できる当社の能力は、数十年にもわたって当社の製造戦略の基礎となっており、多くの場合、製品の再認定を必要とせずに、拠点間でフローを移動することができます。これを踏まえ、当社は、絶えず変化する地政学的環境においてお客様のサプライ チェーンのリスクとコストへの影響を軽減することを目的とした、特殊な製造フローの代替型番 (APN) を提供できるようになりました。特定の国に輸入される TI 製品について、お客様は以下の詳細を考慮することができます。
This search provides import/export information for TI parts such as Harmonized Tariff Schedule (HTS), Export Control Classification Numbers (ECCN) and Country of Origin (COO) specific to the ship to country.
We are constantly enhancing our self-service features, in an effort to provide the most convenient customer experiences. We're pleased to offer search functionality for ".A" APNs today, and are in the process of creating the same functionality for additional specialized flows.
Products based on specialized manufacturing flows
| Suffix | Description | |||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|
| .A | Alternate part numbers with a ”.A” suffix use a wafer fabricated in the U.S. and can be imported into the U.S. without potential future tariff impact. | |||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| .B | Alternate part numbers with a ”.B” suffix can be imported into China without potential future tariff impact. | |||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
| TI may offer additional suffixes in the future, to offer unique manufacturing location flows. | ||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
What to consider when choosing a specialized flow
- These specialized flows are offered as alternate part numbers (APNs) within our existing portfolio, to mitigate future potential tariff impact.
- Some products with specialized flows have an associated cost premium, and come with an extended change order window (COW) of either 42 days (for products that have a published 14- or 42-day COW) or 91 days (for products that have a published 91-day COW).
- Specialized product flows are available for TI’s direct customers to purchase through our backlog channel, and will soon be available through our authorized distributors.
- At the time of shipment, TI will include relevant documentation supporting COO.
- If a tariff is due for any reason upon importation to the specified country, the customer may reject the order and work with TI on shipment-specific options for a return.*
*Additional terms and conditions apply, as set out in our Terms of Sale.
Analysis of potential tariff impact is based on the then-current application of laws of the relevant country. Final tariff determination may be affected by changes in interpretation of such laws or introduction of new laws by relevant authorities. The information provided by TI is for informational purposes and shall not be construed as a representation or warranty of TI.