The 44h01.exe contains a stand-alone WinHelp(TM) datasheet, which describes the functionality of the TPIC44H01 4-Channel Serial and Parallel High-Side Pre-fet Driver.  This product is a stand-alone help file with hypertext links that will run in a Windows(TM) environment.  Help files do not require the user to load a viewer in order to observe the content of the file.  When the 44h01.exe is initiated, a program group will be added to your system called TPIC44H01, and three files will be placed in that group, the TPIC44H01 WinHelp (44h01hlp.hlp 2,096KB) and the TPIC44H01 Uninstall (uninstall.exe 101KB), and this readme file.  These files are defaulted to load to the C: drive under a 44h01 directory.  

To open the TPIC44H01 WinHelp file:  go to Start/TPIC44H01/TPIC44H01 WinHelp

While WinHelp files are MS Windows based, a Windows environment can be immolated on a Unix(TM) operating system.  There are several applications on the market that can achieve this task.  The TPIC44H01 was tested at TI(TM), on a Unix operating system, using WinCenter(R).


"Windows" is a trademark of Microsoft Corporation.
"WinCenter" is registered with NCD.
"WinHelp" is a trademark of Blue Sky Software.
"UNIX" is a trademark of Novell, Inc. in the United States, licensed exclusively through X/Open Company Limited.
"TI" is a trademark of Texas Instruments Incorporated.