Welcome to the software files for the ADS8361 to TMS320F2812!

There are two project files in each of the folders McBSP, SPI and Both.  Mode II and IV are explored using the McBSP port alone, as well as the SPI port.  These projects are located in the SPI and McBSP folders.  

Modes I and III are explored using both McBSP and SPI.  In Mode I, the M0 and M1 pins are controlled by use of the jumper on the evaluation module.  A0 is controlled by the DX pin of the McBSP port.  In Mode III, the A0, M0 and M1 pins are controlled via GPIO functions of PortF.

The "SRC", "CMD" and "INCLUDE" files in the archive are from "C28x Peripheral Examples in C" (document # SPRC097).  If you have questions about this or other Data Converter products, feel free to e-mail us at: 

dataconvapps@list.ti.com

Regards,
Tom Hendrick
Data Acquisition Products - Applications