The following files are included:
1.  Config1cfg_c.c
2.  functions.c
3.  main.c
4.  Config1.cdb
5.  Config1cfg.h
6.  dc_conf.h
7.  Config1cfg.h62
8.  Debug.lkv
9.  ADS8382_C6713DSK.paf
10. ADS8382_C6713DSK.pjt
11. Config1cfg.s62
12. readme.txt
13. Config1cfg.cmd
14.  ads8382_C6713DSK.wks


Directions:
1. Unzip these files into a new directory.  
2. Start Code Composer Studio.  
3. Click on the "File" menu, then click on "Workspace" menu item.
4. Find the directory where these files are stored in.  
5. Select ads8382_C6713DSK.wks, and click "Open"
6. Click on "Project", then click on "Rebuild All"
7. Once the source code is compiled, Click  "File" menu, 
   click "Load Program", find and load "ADS8382_C6713DSK.out".
9. Click "Debug" menu, then click  "Run" menu item.

Assuming a analog input has been applied to the converter channel, the user can observe the digital code in code composer studio's graphical display.