![]() |
![]() |
Configurations for the MSP430 Replicator.
Definition in file Config430.h.

Go to the source code of this file.
Macros | |
| #define | INTERFACE SPYBIWIRE_IF |
| Select the interface to be used to communicate with the device. More... | |
| #define | VCC_LEVEL 30 |
| Set the target's Vcc level supplied by REP430F. More... | |
| #define | MCLK_18MHZ |
| Select the main clock frequency. More... | |
| #define | WordBufferSize 50 |
| Buffer size in words for read and write operations. More... | |
| #define | MAX_ENTRY_TRY 7 |
| Maximum number of tries for the determination of the core identification info. More... | |
| #define | __BYTEWORD__ |
| Comment in the following define if target device is from the ixx family. More... | |
Typedefs | |
| typedef unsigned short | word |
| typedef unsigned char | byte |
Functions | |
| void | runProgramm (void) |
| The basic Replicator routine. More... | |
| void | main (void) |
| Main function. More... | |
| #define __BYTEWORD__ |
Comment in the following define if target device is from the ixx family.
Definition at line 95 of file Config430.h.
| #define INTERFACE SPYBIWIRE_IF |
Select the interface to be used to communicate with the device.
Options:
Select ONLY ONE interface, comment-out remaining options
Definition at line 65 of file Config430.h.
| #define MAX_ENTRY_TRY 7 |
Maximum number of tries for the determination of the core identification info.
Definition at line 86 of file Config430.h.
| #define MCLK_18MHZ |
Select the main clock frequency.
Comment it out for MCLK=12MHz, if the Voltage supplied to the REP430F is low (below 2.5V). That can apply when the REP430F is supplied from the target device, not from the external power supply.
Definition at line 81 of file Config430.h.
| #define VCC_LEVEL 30 |
Set the target's Vcc level supplied by REP430F.
data = 10*Vcc - range 2.1V to 3.6V or 0 (Vcc-OFF)
Definition at line 70 of file Config430.h.
| #define WordBufferSize 50 |
Buffer size in words for read and write operations.
Definition at line 83 of file Config430.h.
| void main | ( | void | ) |
Main function.
Definition at line 119 of file Replicator430.c.

| void runProgramm | ( | void | ) |
The basic Replicator routine.
This function is executed once at startup and can be restarted by pressing button "S1" on the REP430F board.
Data pointer
Buffer, used for memory read with ReadMemQuick()
Data pointer
Buffer, used for memory read with ReadMemQuick()
Definition at line 127 of file Replicator430.c.