![]() |
![]() |
JTAG Function Prototypes and Definitions.
Definition in file JTAGfunc430.h.
#include "Config430.h"

Go to the source code of this file.
Macros | |
| #define | IR_CNTRL_SIG_16BIT 0xC8 |
| Set the JTAG control signal register. More... | |
| #define | IR_CNTRL_SIG_CAPTURE 0x28 |
| Read out the JTAG control signal register. More... | |
| #define | IR_CNTRL_SIG_RELEASE 0xA8 |
| Release the CPU from JTAG control. More... | |
| #define | IR_PREPARE_BLOW 0x44 |
| Prepare for JTAG fuse blow. More... | |
| #define | IR_EX_BLOW 0x24 |
| Perform JTAG fuse blow. More... | |
| #define | IR_DATA_16BIT 0x82 |
| Set the MSP430 MDB to a specific 16-bit value with the next 16-bit data access. More... | |
| #define | IR_DATA_QUICK 0xC2 |
| Set the MSP430 MDB to a specific 16-bit value (RAM only) More... | |
| #define | IR_DATA_PSA 0x22 |
| Switch JTAG data register to PSA mode. More... | |
| #define | IR_SHIFT_OUT_PSA 0x62 |
| Shift out the PSA pattern generated by IR_DATA_PSA. More... | |
| #define | IR_ADDR_16BIT 0xC1 |
| Set the MSP430 MAB to a specific 16-bit value. More... | |
| #define | IR_ADDR_CAPTURE 0x21 |
| Read out the MAB data on the next 16/20-bit data access. More... | |
| #define | IR_DATA_TO_ADDR 0xA1 |
| Set the MSP430 MDB with a specific 16-bit value and write it to the memory address which is currently on the MAB. More... | |
| #define | IR_BYPASS 0xFF |
| Bypass instruction - TDI input is shifted to TDO as an output. More... | |
| #define | JTAG_ID 0x89 |
| JTAG identification value for MSP430 architecture devices. More... | |
| #define | F_BYTE 8 |
| #define | F_WORD 16 |
| #define | V_RESET 0xFFFE |
| #define | VPP_ON_TDI 0 |
| Fuse blow voltage is supplied via the TDI pin. More... | |
| #define | VPP_ON_TEST 1 |
| Fuse blow voltage is supplied via the TEST pin. More... | |
Functions | |
| word | DR_Shift16 (word Data) |
| Function for shifting a given 16-bit word into the JTAG data register through TDI. More... | |
| word | IR_Shift (byte Instruction) |
| Function for shifting a new instruction into the JTAG instruction register through TDI (MSB first, but with interchanged MSB - LSB, to simply use the same shifting function, Shift(), as used in DR_Shift16). More... | |
| void | ResetTAP (void) |
| Reset target JTAG interface and perform fuse-HW check. More... | |
| word | ExecutePOR (void) |
| Function to execute a Power-On Reset (POR) using JTAG CNTRL SIG register. More... | |
| word | SetInstrFetch (void) |
| Function to set target CPU JTAG FSM into the instruction fetch state. More... | |
| void | SetPC (word Addr) |
| Load a given address into the target CPU's program counter (PC). More... | |
| void | HaltCPU (void) |
| Function to set the CPU into a controlled stop state. More... | |
| void | ReleaseCPU (void) |
| Function to release the target CPU from the controlled stop state. More... | |
| word | VerifyPSA (word StartAddr, word Length, word *DataArray) |
| word | GetDevice (void) |
| Function to take target device under JTAG control. Disables the target watchdog. Sets the global DEVICE variable as read from the target device. More... | |
| void | ReleaseDevice (word Addr) |
| Function to release the target device from JTAG control. More... | |
| void | WriteMem (word Format, word Addr, word Data) |
| This function writes one byte/word at a given address ( <0xA00) More... | |
| void | WriteMemQuick (word StartAddr, word Length, word *DataArray) |
| This function writes an array of words into the target memory. More... | |
| void | WriteFLASH (word StartAddr, word Length, word *DataArray) |
| This function programs/verifies an array of words into the FLASH memory by using the FLASH controller. More... | |
| word | WriteFLASHallSections (const unsigned int *data, const unsigned long *address, const unsigned long *length_of_sections, const unsigned long sections) |
| This function programs/verifies a set of data arrays of words into a FLASH memory by using the "WriteFLASH()" function. It conforms with the "CodeArray" structure convention of file "Target_Code_(IDE).s43" or "Target_Code.h". More... | |
| word | ReadMem (word Format, word Addr) |
| This function reads one byte/word from a given address in memory. More... | |
| void | ReadMemQuick (word StartAddr, word Length, word *DataArray) |
| This function reads an array of words from the memory. More... | |
| void | EraseFLASH (word EraseMode, word EraseAddr) |
| This function performs a mass erase (with and w/o info memory) or a segment erase of a FLASH module specified by the given mode and address. Large memory devices get additional mass erase operations to meet the spec. (Could be extended with erase check via PSA) More... | |
| word | EraseCheck (word StartAddr, word Length) |
| This function performs an Erase Check over the given memory range. More... | |
| word | VerifyMem (word StartAddr, word Length, word *DataArray) |
| This function performs a Verification over the given memory range. More... | |
| word | BlowFuse (void) |
| This function blows the security fuse. More... | |
| word | IsFuseBlown (void) |
| This function checks if the JTAG access security fuse is blown. More... | |
| void | UnlockInfoA (void) |
| This Function unlocks segment A of the InfoMemory (Flash) More... | |
| #define IR_ADDR_16BIT 0xC1 |
Set the MSP430 MAB to a specific 16-bit value.
Use the 20-bit macro for 430X and 430Xv2 architectures
Definition at line 112 of file JTAGfunc430.h.
| #define IR_ADDR_CAPTURE 0x21 |
Read out the MAB data on the next 16/20-bit data access.
Definition at line 114 of file JTAGfunc430.h.
| #define IR_BYPASS 0xFF |
Bypass instruction - TDI input is shifted to TDO as an output.
Definition at line 119 of file JTAGfunc430.h.
| #define IR_CNTRL_SIG_16BIT 0xC8 |
Set the JTAG control signal register.
Definition at line 84 of file JTAGfunc430.h.
| #define IR_CNTRL_SIG_CAPTURE 0x28 |
Read out the JTAG control signal register.
Definition at line 86 of file JTAGfunc430.h.
| #define IR_CNTRL_SIG_RELEASE 0xA8 |
Release the CPU from JTAG control.
Definition at line 88 of file JTAGfunc430.h.
| #define IR_DATA_16BIT 0x82 |
Set the MSP430 MDB to a specific 16-bit value with the next 16-bit data access.
Definition at line 99 of file JTAGfunc430.h.
| #define IR_DATA_PSA 0x22 |
Switch JTAG data register to PSA mode.
Definition at line 105 of file JTAGfunc430.h.
| #define IR_DATA_QUICK 0xC2 |
Set the MSP430 MDB to a specific 16-bit value (RAM only)
Definition at line 101 of file JTAGfunc430.h.
| #define IR_DATA_TO_ADDR 0xA1 |
Set the MSP430 MDB with a specific 16-bit value and write it to the memory address which is currently on the MAB.
Definition at line 117 of file JTAGfunc430.h.
| #define IR_EX_BLOW 0x24 |
Perform JTAG fuse blow.
Definition at line 94 of file JTAGfunc430.h.
| #define IR_PREPARE_BLOW 0x44 |
Prepare for JTAG fuse blow.
Definition at line 92 of file JTAGfunc430.h.
| #define IR_SHIFT_OUT_PSA 0x62 |
Shift out the PSA pattern generated by IR_DATA_PSA.
Definition at line 107 of file JTAGfunc430.h.
| #define JTAG_ID 0x89 |
JTAG identification value for MSP430 architecture devices.
Definition at line 123 of file JTAGfunc430.h.
| #define VPP_ON_TDI 0 |
Fuse blow voltage is supplied via the TDI pin.
Definition at line 132 of file JTAGfunc430.h.
| #define VPP_ON_TEST 1 |
Fuse blow voltage is supplied via the TEST pin.
Definition at line 134 of file JTAGfunc430.h.
| word BlowFuse | ( | void | ) |
This function blows the security fuse.
Definition at line 1240 of file JTAGfunc430.c.

| word DR_Shift16 | ( | word | data | ) |
Function for shifting a given 16-bit word into the JTAG data register through TDI.
| [in] | word | data (16-bit data, MSB first) |
Definition at line 94 of file JTAGfunc430.c.

| word EraseCheck | ( | word | StartAddr, |
| word | Length | ||
| ) |
This function performs an Erase Check over the given memory range.
| [in] | word | StartAddr (Start address of memory to be checked) |
| [in] | word | Length (Number of words to be checked) |
Definition at line 1220 of file JTAGfunc430.c.
| void EraseFLASH | ( | word | EraseMode, |
| word | EraseAddr | ||
| ) |
This function performs a mass erase (with and w/o info memory) or a segment erase of a FLASH module specified by the given mode and address. Large memory devices get additional mass erase operations to meet the spec. (Could be extended with erase check via PSA)
| [in] | word | Mode (could be ERASE_MASS or ERASE_MAIN or ERASE_SGMT) |
| [in] | word | Addr (any address within the selected segment) |
Definition at line 1044 of file JTAGfunc430.c.

| word ExecutePOR | ( | void | ) |
Function to execute a Power-On Reset (POR) using JTAG CNTRL SIG register.
Definition at line 239 of file JTAGfunc430.c.

| word GetDevice | ( | void | ) |
Function to take target device under JTAG control. Disables the target watchdog. Sets the global DEVICE variable as read from the target device.
Definition at line 659 of file JTAGfunc430.c.

| void HaltCPU | ( | void | ) |
Function to set the CPU into a controlled stop state.
Definition at line 311 of file JTAGfunc430.c.

| word IR_Shift | ( | byte | instruction | ) |
Function for shifting a new instruction into the JTAG instruction register through TDI (MSB first, but with interchanged MSB - LSB, to simply use the same shifting function, Shift(), as used in DR_Shift16).
| [in] | byte | Instruction (8bit JTAG instruction, MSB first) |
Definition at line 137 of file JTAGfunc430.c.

| word IsFuseBlown | ( | void | ) |
This function checks if the JTAG access security fuse is blown.
Definition at line 1290 of file JTAGfunc430.c.

| word ReadMem | ( | word | Format, |
| word | Addr | ||
| ) |
This function reads one byte/word from a given address in memory.
| [in] | word | Format (F_BYTE or F_WORD) |
| [in] | word | Addr (address of memory) |
Definition at line 980 of file JTAGfunc430.c.

| void ReadMemQuick | ( | word | StartAddr, |
| word | Length, | ||
| word * | DataArray | ||
| ) |
This function reads an array of words from the memory.
| [in] | word | StartAddr (Start address of memory to be read) |
| [in] | word | Length (Number of words to be read) |
| [out] | word | *DataArray (Pointer to array for the data) |
Definition at line 1013 of file JTAGfunc430.c.

| void ReleaseCPU | ( | void | ) |
Function to release the target CPU from the controlled stop state.
Definition at line 325 of file JTAGfunc430.c.

| void ReleaseDevice | ( | word | Addr | ) |
Function to release the target device from JTAG control.
| [in] | word | Addr (0xFFFE: Perform Reset, means Load Reset Vector into PC, otherwise: Load Addr into PC) |
Definition at line 721 of file JTAGfunc430.c.

| void ResetTAP | ( | void | ) |
Reset target JTAG interface and perform fuse-HW check.
Definition at line 180 of file JTAGfunc430.c.

| word SetInstrFetch | ( | void | ) |
Function to set target CPU JTAG FSM into the instruction fetch state.
Definition at line 267 of file JTAGfunc430.c.

| void SetPC | ( | word | Addr | ) |
Load a given address into the target CPU's program counter (PC).
| [in] | word | Addr (destination address) |
Definition at line 289 of file JTAGfunc430.c.

| void UnlockInfoA | ( | void | ) |
This Function unlocks segment A of the InfoMemory (Flash)
Definition at line 1307 of file JTAGfunc430.c.
| word VerifyMem | ( | word | StartAddr, |
| word | Length, | ||
| word * | DataArray | ||
| ) |
This function performs a Verification over the given memory range.
| [in] | word | StartAddr (Start address of memory to be verified) |
| [in] | word | Length (Number of words to be verified) |
| [in] | word | *DataArray (Pointer to array with the data) |
Definition at line 1232 of file JTAGfunc430.c.
| void WriteFLASH | ( | word | StartAddr, |
| word | Length, | ||
| word * | DataArray | ||
| ) |
This function programs/verifies an array of words into the FLASH memory by using the FLASH controller.
| [in] | word | StartAddr (Start address of FLASH memory) |
| [in] | word | Length (Number of words to be programmed) |
| [in] | word | *DataArray (Pointer to array with the data) |
Definition at line 797 of file JTAGfunc430.c.

| word WriteFLASHallSections | ( | const unsigned int * | data, |
| const unsigned long * | address, | ||
| const unsigned long * | length_of_sections, | ||
| const unsigned long | sections | ||
| ) |
This function programs/verifies a set of data arrays of words into a FLASH memory by using the "WriteFLASH()" function. It conforms with the "CodeArray" structure convention of file "Target_Code_(IDE).s43" or "Target_Code.h".
| [in] | const | unsigned int *DataArray (Pointer to array with the data) |
| [in] | const | unsigned long *address (Pointer to array with the startaddresses) |
| [in] | const | unsigned long *length_of_sections (Pointer to array with the number of words counting from startaddress) |
| [in] | const | unsigned long sections (Number of sections in code file) |
Definition at line 957 of file JTAGfunc430.c.

| void WriteMem | ( | word | Format, |
| word | Addr, | ||
| word | Data | ||
| ) |
This function writes one byte/word at a given address ( <0xA00)
| [in] | word | Format (F_BYTE or F_WORD) |
| [in] | word | Addr (Address of data to be written) |
| [in] | word | Data (shifted data) |
Definition at line 741 of file JTAGfunc430.c.

| void WriteMemQuick | ( | word | StartAddr, |
| word | Length, | ||
| word * | DataArray | ||
| ) |
This function writes an array of words into the target memory.
| [in] | word | StartAddr (Start address of target memory) |
| [in] | word | Length (Number of words to be programmed) |
| [in] | word | *DataArray (Pointer to array with the data) |
Definition at line 769 of file JTAGfunc430.c.