![]() |
![]() |
JTAG Control Sequences for Erasing / Programming / Fuse Burning.
Definition in file JTAGfunc430X.c.

Go to the source code of this file.
Functions | |
| word | VerifyPSA_430X (unsigned long StartAddr, unsigned long Length, word *DataArray) |
| This function compares the computed PSA (Pseudo Signature Analysis) value to the PSA value shifted out from the target device. It is used for very fast data block write or erasure verification. More... | |
| word | GetDevice_430X (void) |
| Function to take target device under JTAG control. Disables the target watchdog. Sets the global DEVICE variable as read from the target device. More... | |
| void | ReleaseDevice_430X (unsigned long Addr) |
| Function to release the target device from JTAG control. More... | |
| void | WriteMem_430X (word Format, unsigned long Addr, word Data) |
| This function writes one byte/word at a given address ( <0xA00) More... | |
| void | WriteMemQuick_430X (unsigned long StartAddr, unsigned long Length, word *DataArray) |
| This function writes an array of words into the target memory. More... | |
| void | WriteFLASH_430X (unsigned long StartAddr, unsigned long Length, word *DataArray) |
| This function programs/verifies an array of words into the FLASH memory by using the FLASH controller. More... | |
| word | WriteFLASHallSections_430X (const unsigned int *data, const unsigned long *address, const unsigned long *length_of_sections, const unsigned long sections) |
| This function programs/verifies a set of data arrays of words into a FLASH memory by using the "WriteFLASH()" function. It conforms with the "CodeArray" structure convention of file "Target_Code_(IDE).s43" or "Target_Code.h". More... | |
| word | ReadMem_430X (word Format, unsigned long Addr) |
| This function reads one byte/word from a given address in memory. More... | |
| void | ReadMemQuick_430X (unsigned long StartAddr, unsigned long Length, word *DataArray) |
| This function reads an array of words from the memory. More... | |
| void | EraseFLASH_430X (word EraseMode, unsigned long EraseAddr) |
| This function performs a mass erase (with and w/o info memory) or a segment erase of a FLASH module specified by the given mode and address. Large memory devices get additional mass erase operations to meet the spec. (Could be extended with erase check via PSA) More... | |
| word | EraseCheck_430X (unsigned long StartAddr, unsigned long Length) |
| This function performs an Erase Check over the given memory range. More... | |
| word | VerifyMem_430X (unsigned long StartAddr, unsigned long Length, word *DataArray) |
| This function performs a Verification over the given memory range. More... | |
| word | BlowFuse (void) |
| This function blows the security fuse. More... | |
| word | IsFuseBlown (void) |
| This function checks if the JTAG access security fuse is blown. More... | |
| void | UnlockInfoA (void) |
| This function unlocks segment A of the InfoMemory (Flash) More... | |
| word BlowFuse | ( | void | ) |
This function blows the security fuse.
Definition at line 1038 of file JTAGfunc430X.c.

| word EraseCheck_430X | ( | unsigned long | StartAddr, |
| unsigned long | Length | ||
| ) |
This function performs an Erase Check over the given memory range.
| [in] | word | StartAddr (Start address of memory to be checked) |
| [in] | word | Length (Number of words to be checked) |
Definition at line 1018 of file JTAGfunc430X.c.

| void EraseFLASH_430X | ( | word | EraseMode, |
| unsigned long | EraseAddr | ||
| ) |
This function performs a mass erase (with and w/o info memory) or a segment erase of a FLASH module specified by the given mode and address. Large memory devices get additional mass erase operations to meet the spec. (Could be extended with erase check via PSA)
| [in] | word | Mode (could be ERASE_MASS or ERASE_MAIN or ERASE_SGMT) |
| [in] | word | Addr (any address within the selected segment) |
Definition at line 932 of file JTAGfunc430X.c.

| word GetDevice_430X | ( | void | ) |
Function to take target device under JTAG control. Disables the target watchdog. Sets the global DEVICE variable as read from the target device.
Definition at line 632 of file JTAGfunc430X.c.

| word IsFuseBlown | ( | void | ) |
This function checks if the JTAG access security fuse is blown.
Definition at line 1072 of file JTAGfunc430X.c.
| word ReadMem_430X | ( | word | Format, |
| unsigned long | Addr | ||
| ) |
This function reads one byte/word from a given address in memory.
| [in] | word | Format (F_BYTE or F_WORD) |
| [in] | word | Addr (address of memory) |
Definition at line 871 of file JTAGfunc430X.c.
| void ReadMemQuick_430X | ( | unsigned long | StartAddr, |
| unsigned long | Length, | ||
| word * | DataArray | ||
| ) |
This function reads an array of words from the memory.
| [in] | word | StartAddr (Start address of memory to be read) |
| [in] | word | Length (Number of words to be read) |
| [out] | word | *DataArray (Pointer to array for the data) |
Definition at line 902 of file JTAGfunc430X.c.
| void ReleaseDevice_430X | ( | unsigned long | Addr | ) |
Function to release the target device from JTAG control.
| [in] | word | Addr (0xFFFE: Perform Reset, means Load Reset Vector into PC, otherwise: Load Addr into PC) |
Definition at line 693 of file JTAGfunc430X.c.
| void UnlockInfoA | ( | void | ) |
This function unlocks segment A of the InfoMemory (Flash)
Definition at line 1089 of file JTAGfunc430X.c.
| word VerifyMem_430X | ( | unsigned long | StartAddr, |
| unsigned long | Length, | ||
| word * | DataArray | ||
| ) |
This function performs a Verification over the given memory range.
| [in] | word | StartAddr (Start address of memory to be verified) |
| [in] | word | Length (Number of words to be verified) |
| [in] | word | *DataArray (Pointer to array with the data) |
Definition at line 1030 of file JTAGfunc430X.c.

| word VerifyPSA_430X | ( | unsigned long | StartAddr, |
| unsigned long | Length, | ||
| word * | DataArray | ||
| ) |
This function compares the computed PSA (Pseudo Signature Analysis) value to the PSA value shifted out from the target device. It is used for very fast data block write or erasure verification.
| [in] | unsigned | long StartAddr (Start address of data block to be checked) |
| [in] | unsigned | long Length (Number of words within data block) |
| [in] | word | *DataArray (Pointer to array with the data, 0 for Erase Check) |
Definition at line 378 of file JTAGfunc430X.c.

| void WriteFLASH_430X | ( | unsigned long | StartAddr, |
| unsigned long | Length, | ||
| word * | DataArray | ||
| ) |
This function programs/verifies an array of words into the FLASH memory by using the FLASH controller.
| [in] | word | StartAddr (Start address of FLASH memory) |
| [in] | word | Length (Number of words to be programmed) |
| [in] | word | *DataArray (Pointer to array with the data) |
Definition at line 768 of file JTAGfunc430X.c.

| word WriteFLASHallSections_430X | ( | const unsigned int * | data, |
| const unsigned long * | address, | ||
| const unsigned long * | length_of_sections, | ||
| const unsigned long | sections | ||
| ) |
This function programs/verifies a set of data arrays of words into a FLASH memory by using the "WriteFLASH()" function. It conforms with the "CodeArray" structure convention of file "Target_Code_(IDE).s43" or "Target_Code.h".
| [in] | const | unsigned int *DataArray (Pointer to array with the data) |
| [in] | const | unsigned long *address (Pointer to array with the startaddresses) |
| [in] | const | unsigned long *length_of_sections (Pointer to array with the number of words counting from startaddress) |
| [in] | const | unsigned long sections (Number of sections in code file) |
Definition at line 848 of file JTAGfunc430X.c.
| void WriteMem_430X | ( | word | Format, |
| unsigned long | Addr, | ||
| word | Data | ||
| ) |
This function writes one byte/word at a given address ( <0xA00)
| [in] | word | Format (F_BYTE or F_WORD) |
| [in] | word | Addr (Address of data to be written) |
| [in] | word | Data (shifted data) |
Definition at line 713 of file JTAGfunc430X.c.
| void WriteMemQuick_430X | ( | unsigned long | StartAddr, |
| unsigned long | Length, | ||
| word * | DataArray | ||
| ) |
This function writes an array of words into the target memory.
| [in] | word | StartAddr (Start address of target memory) |
| [in] | word | Length (Number of words to be programmed) |
| [in] | word | *DataArray (Pointer to array with the data) |
Definition at line 741 of file JTAGfunc430X.c.