How to use these files with Code Composer Studio:

1) First Setup the Code Composer Studio with the appropriate Board type/name, I/O port,
   CPU type and GEL file
2) Start Code Composer Studio and create a new project by selecting Project-New from
   the menu and then select the location and name of the project on the computer
3) From the menu, select Project-Build Options-Target and then on the Compiler Tab choose
   the appropriate device form the Basic-Target Version
4) From the menu choose Project-Add Files to Project and add the appropriate
   source files. Also include the library files (*.lib) from C:\ti according
   to the target C6000 device used
5) In the same way, add the appropriate lnk.cmd file to the project.  This linker
   command file is specifically configured for the C6711 DSK.  You must modify
   the file to run the program on a different DSP.
5) In the source file change the #define CHIP_6xxx to the appropriate
   number according to the TMS320C6000 DSP used. For instance if the TMS320C6711 is
   used change the code to #define CHIP_6711
6) Build the project by selecting Project-Build from the menu
7) Load the program by selecting File-Load Program from the menu
8) Run the program