Note: These GELs are an adaptation of the internal GEL framework, modified for use/distribution to customers via the CSP. 

To initialize clocks and ddr run the tests:
	 DO "~~~~/j7es_m3.cmm" 
	 DO "~~~~/J721E.cmm"

After these menus to test the system will be installed.

It will be possible to attach to each core after the clocks/power is on by calling:
	j7es_a72.cmm
	j7es_c7x.cmm
	j7es_c66.cmm
	j7es_icssg.cmm
	j7es_m3.cmm
	j7es_r5.cmm

A ddr test executed from the A72 can be auto run by calling:
	dra829_a72_ddr_test.cmm