# PRU_CGT environment variable must point to the TI PRU code gen tools directory. E.g.:
#(Desktop Linux) export PRU_CGT=/path/to/pru/code/gen/tools/ti-cgt-pru_2.x.y
#(Windows) set PRU_CGT=C:/path/to/pru/code/gen/tools/ti-cgt-pru_2.x.y
#(ARM Linux*) export PRU_CGT=/usr/share/ti/cgt-pru
#
# *ARM Linux also needs to create a symbolic link to the /usr/bin/ directory in
# order to use the same Makefile
#(ARM Linux) ln -s /usr/bin/ /usr/share/ti/cgt-pru/bin

ifndef PRU_CGT
define ERROR_BODY

*******************************************************************************
PRU_CGT environment variable is not set. Examples given:
(Desktop Linux) export PRU_CGT=/path/to/pru/code/gen/tools/ti-cgt-pru_2.1.2
(Windows) set PRU_CGT=C:/path/to/pru/code/gen/tools/ti-cgt-pru_2.1.2
(ARM Linux*) export PRU_CGT=/usr/share/ti/cgt-pru

*ARM Linux also needs to create a symbolic link to the /usr/bin/ directory in
order to use the same Makefile
(ARM Linux) ln -s /usr/bin/ /usr/share/ti/cgt-pru/bin
*******************************************************************************

endef
$(error $(ERROR_BODY))
endif

MKFILE_PATH := $(abspath $(lastword $(MAKEFILE_LIST)))
CURRENT_DIR := $(notdir $(patsubst %/,%,$(dir $(MKFILE_PATH))))
PROJ_NAME=sddf

LINKER_COMMAND_FILE=./ICSSG_PRU.cmd

LIBS=

#INCLUDE=--include_path="./"
STACK_SIZE=0x100
HEAP_SIZE=0x100
GEN_DIR=gen

#CDEFINES = -DSOC_AM65XX
CDEFINES = -DSOC_AM64X

#Common compiler and linker flags (Defined in 'PRU Optimizing C/C++ Compiler User's Guide)
CFLAGS= $(CDEFINES) -v3 -o2 --display_error_number --endian=little --hardware_mac=on --asm_directory=$(GEN_DIR) --obj_directory=$(GEN_DIR) --pp_directory=$(GEN_DIR) -ppd -ppa
#Linker flags (Defined in 'PRU Optimizing C/C++ Compiler User's Guide)
LFLAGS=--reread_libs --warn_sections --stack_size=$(STACK_SIZE) --heap_size=$(HEAP_SIZE) --entry_point=SDDF_ENTRY


TARGET=$(GEN_DIR)/$(PROJ_NAME)_array.h
PRU_IMAGE_PREFIX=pru_$(PROJ_NAME)_image

EXE=$(GEN_DIR)/$(PROJ_NAME).out
MAP=$(GEN_DIR)/$(PROJ_NAME).map
OBJECTS=$(patsubst %.asm,$(GEN_DIR)/%.object,$(wildcard *.asm))
OBJECTS+=$(patsubst %.c,$(GEN_DIR)/%.object,$(wildcard *.c))


all: printStart $(TARGET) printEnd

printStart:
	@echo ''
	@echo '************************************************************'
	@echo 'Building project: $(PROJ_NAME)'

printEnd:
	@echo ''
	@echo 'Output files can be found in the "$(GEN_DIR)" directory'
	@echo ''
	@echo 'Finished building project: $(PROJ_NAME)'
	@echo '************************************************************'
	@echo ''


# Invoke the hex format converter to translate the .out file to a C header file
$(TARGET): $(EXE)
	@echo ''
	@echo 'Building image header file: $@'
	@echo 'Invoking: PRU Hex Format Converter'
	$(PRU_CGT)/bin/hexpru --array --array:name_prefix=$(PRU_IMAGE_PREFIX) $(EXE)
	mv $(subst .h,.c,$(PROJ_NAME)_array.h) $(TARGET)
	@echo 'Finished image header file: $@'
    
# Invokes the linker (-z flag) to make the .out file
$(EXE): $(OBJECTS) $(LINKER_COMMAND_FILE)
	@echo ''
	@echo 'Building executable: $@'
	@echo 'Invoking: PRU Linker'
#	$(PRU_CGT)/bin/clpru $(CFLAGS) -z -i$(PRU_CGT)/lib -i$(PRU_CGT)/include $(LFLAGS) -o $(EXE) $(OBJECTS) -m$(MAP) $(LINKER_COMMAND_FILE) --library=libc.a $(LIBS)
	$(PRU_CGT)/bin/clpru $(CFLAGS) -z -i$(PRU_CGT)/lib -i$(PRU_CGT)/include $(LFLAGS) -o $(EXE) $(OBJECTS) -m$(MAP) $(LINKER_COMMAND_FILE) $(LIBS)
	@echo 'Finished building executable: $@'

# Invokes the compiler on all assembly files in the directory to create the object files
$(GEN_DIR)/%.object: %.asm
	@mkdir -p $(GEN_DIR)
	@echo ''
	@echo 'Building file: $<'
	@echo 'Invoking: PRU Compiler'
	$(PRU_CGT)/bin/clpru --include_path=$(PRU_CGT)/include $(INCLUDE) $(CFLAGS) -fe $@ $<

# Invokes the compiler on all c files in the directory to create the object files
$(GEN_DIR)/%.object: %.c
	@mkdir -p $(GEN_DIR)
	@echo ''
	@echo 'Building file: $<'
	@echo 'Invoking: PRU Compiler'
	$(PRU_CGT)/bin/clpru -k --include_path=$(PRU_CGT)/include $(INCLUDE) $(CFLAGS) -fe $@ $<

.PHONY: all clean

# Remove the $(GEN_DIR) directory
clean:
	@echo ''
	@echo '************************************************************'
	@echo 'Cleaning project: $(PROJ_NAME)'
	@echo ''
	@echo 'Removing files in the "$(GEN_DIR)" directory'
	@rm -rf $(GEN_DIR)
	@rm -f $(subst .h,.c,$(PROJ_NAME)_array.h)
	@echo ''
	@echo 'Finished cleaning project: $(PROJ_NAME)'
	@echo '************************************************************'
	@echo ''

# Includes the dependencies that the compiler creates (-ppd and -ppa flags)
-include $(OBJECTS:%.object=%.pp)