Forward Annotation
                               ------------------

                       02:38 PM Wednesday, March 14, 2012
Job Name: C:\Users\a0866685\Documents\Haptics\Devices\DRV2667\EVM\DRV2667EVM-MINI\PCB\DRV2667EVM-MINI.pcb


Version:  01.01.00

     The PDBs listed in the project file will be searched to satisfy the parts
      requirements of the CDB only for parts not already found in the
      Target PDB.

     The schematic source is a Common Data Base.

     The AllowAlphaRefDes status indicates that reference
      designators containing all alpha characters should be respected.

     The FLATNETNAMEs status indicates that the present set
      of schematic netnames should be used to update the
      FLATNETNAMEs.

     The present Common DataBase is up to date with the schematic
      source files.

     Common Data Base has been read

     Target PDB Name: Work\Layout_Temp\PartsDB.pdb

     Number of Part Numbers: 12
          Part Numb: CRCW040213K0FKED -> Vend Part: CRCW040213K0FKED 
          Part Numb: CRCW040235K7FKED -> Vend Part: CRCW040235K7FKED 
          Part Numb: C1206F104K1RACTU -> Vend Part: C1206F104K1RACTU 
          Part Numb: DRV2667RGP -> Vend Part: DRV2667RGP 
          Part Numb: GRM155R60J105KE19D -> Vend Part: GRM155R60J105KE19D 
          Part Numb: GRM155R71C104KA88D -> Vend Part: GRM155R71C104KA88D 
          Part Numb: RC0402FR-07768KL -> Vend Part: RC0402FR-07768KL 
          Part Numb: R0402_DNP -> Vend Part: R0402_DNP 
          Part Numb: TestPoint_TH-40x25 -> Vend Part: TestPoint_TH-40x25 
          Part Numb: VLS3012T-1R0N2R2 -> Vend Part: VLS3012T-1R0N2R2 
          Part Numb: 0805YD106KAT2A -> Vend Part: 0805YD106KAT2A 
          Part Numb: 06033D104KAT2A -> Vend Part: 06033D104KAT2A 

     Number of Part Names: 0

     Number of Part Labels: 0


     Checking for value differences between symbol properties and PartsDB properties

WARNING Block DRV8601CapTouch_RevA Page 1, Symbol XCMP333: Symbol / PartsDB property mismatch
      Resolved PartNumber = VLS3012T-1R0N2R2
      Symbol Property: free2 = 3.3uH/1.1A
     PartsDB Property: free2 = 1.0uH/2.5A

WARNING Block DRV8601CapTouch_RevA Page 1, Symbol XCMP333: Symbol / PartsDB property mismatch
      Resolved PartNumber = VLS3012T-1R0N2R2
      Symbol Property: free1 = VLS3010ET-3R3M
     PartsDB Property: free1 = VLS3012

WARNING Block DRV8601CapTouch_RevA Page 1, Symbol XCMP333: Symbol / PartsDB property mismatch
      Resolved PartNumber = VLS3012T-1R0N2R2
      Symbol Property: VendorPartNum = VLS3010ET-3R3M
     PartsDB Property: VendorPartNum = VLS3012T-1R0N2R2

WARNING Block DRV8601CapTouch_RevA Page 1, Symbol XCMP351: Symbol / PartsDB property mismatch
      Resolved PartNumber = GRM155R71C104KA88D
      Symbol Property: free1 = 0402
     PartsDB Property: free1 = 0402  X7R

WARNING Block DRV8601CapTouch_RevA Page 1, Symbol XCMP350: Symbol / PartsDB property mismatch
      Resolved PartNumber = GRM155R71C104KA88D
      Symbol Property: free1 = 0402
     PartsDB Property: free1 = 0402  X7R

WARNING Block DRV8601CapTouch_RevA Page 1, Symbol XCMP336: Symbol / PartsDB property mismatch
      Resolved PartNumber = GRM155R71C104KA88D
      Symbol Property: free1 = 0402
     PartsDB Property: free1 = 0402  X7R

     Checking the validity of the packaging of prepackaged schematic
      symbols.  Only the first error in symbols having the same
      Reference Designator will be reported.

     The packaging of all prepackaged schematic symbols is consistent
      with the Parts DataBase data for the cross mapping of
      symbol pin names to Part Number pin numbers.
      Symbols that were not prepackaged will now be packaged correctly.
      
     No errors in Existing Schematic Packaging.

     The Common DataBase has been read and will be packaged.
     Clustering 25 Symbols:
              25  ************************
     Clustering is Complete

     Packager Assignments successfully completed



     17 nets were found containing 57 pins
     24 components were found

     After augmentation of supply pins, there are 17 nets where 0 nets have only one pin.

     Creating a formatted Schematic Netlist (LogFiles\SchematicNetlist.txt)...
     A formatted Schematic Netlist has been created.

     The Logic DataBase has been compiled from the Schematic Design.
      Use Netload to bring the Component Design into sync.

     This Logic Data was Compiled with 6 warnings.
      Erroneous results may occur if not fixed.

                                     NetLoad
                                     -------

                       02:38 PM Wednesday, March 14, 2012
Job Name: C:\Users\a0866685\Documents\Haptics\Devices\DRV2667\EVM\DRV2667EVM-MINI\PCB\DRV2667EVM-MINI.pcb


Version:  02.11.12

     Netloading the Layout.  Unused components will be deleted.

     Unconnected pins will be set to net "(Net0)".

     Schematic reference designator changes will be forward annotated.

     Netload completed successfully with 0 warning(s).
     
     Back Annotating...

  Updating Logic Database...

     Version:  99.00.05

     No changes made to Existing Schematic Packaging.


     There is no symbol data to be back annotated to the schematic source.


     The Logic DataBase has been updated and the Common DataBase has
      automatically been brought into sync with the Logic DataBase.
      Please proceed with your design.

     Finished updating the Logic Database.

     Creating a formatted Schematic Netlist (LogFiles\AfterBakAnnoNetlist.txt)...
     A formatted Schematic Netlist has been created.

     Creating a new netlist text file (LogFiles\KeyinNetList.txt)
      from the Logic Database (Work\Layout_Temp\LogicDB.lgc)...
  A new netlist text file has been generated.



                 Beginning Netload on the Layout Design.
           ---------------------------------------------------

Forward-Annotation on the Layout Design has been successfully completed.

There were 0 reassignments of nets.
There were 0 traces broken back.
There were 0 nets removed from the Layout Design.