How can I add or change addresses in my account address book?

To add or edit an address:

  1. Log in to your myTI account dashboard.
  2. Navigate to the left-hand side of myTI dashboard. Under Ordering, select Addresses.
  3. On the Addresses page:
    • To add an address, click the Add new button in the upper right-hand corner.
    • To edit an existing address, click the Pencil icon. (Note that editing an address used in one or more checkout profiles will affect each of those profiles.)
    • To delete an address, click the Delete icon.
  4. Once you are done with your edits, return to the Addresses page to confirm your changes.

You also have the ability to save new address or edit an existing address during checkout. 

Find answers to your ordering questions

Explore other ways to find answers