GPCCHEM

Gauging Parameter Calculator: Match chemistry for Impedance Track gauges

GPCCHEM

Overview

GPC Chemistry ID matching for Impedance Track (IT) algorithm gas gauges (Find closest chemistry match) must be done before Optimizing room temperature or low temperature performance.

Gauging Parameter Calculator Chemistry ID matching for Impedance track gas gauges (GPCCHEM) is a math calculation and simulation tool that helps the battery designer to obtain matching chemistry ID for the specific battery profile. Chemistry IDs are defined by Texas Instruments and can be programmed using Battery Management Studio (bqStudio). The GPCCHEM tool allows the user to increase the accuracy of the fuel gauge IC.

The battery pack must use one of TI’s Impedance Track(IT) algorithm based fuel gauges. It accepts log files in the format specified in the instruction manual. The log files can be created by using TI’s Battery Management Studio (bqStudio) software with the specific Evaluation board connected through USB, or by any battery tester with data logging capabilities like Arbin or Maccor. External equipment is required for charge and discharge. For accurate calculations it will also require additional parameters of the battery pack setup. The output information will be emailed as a text file containing the Chemistry ID. The chemistry ID data can be programmed into Data Flash using bqStudio to create a golden image that can be used in mass production of battery packs.

If bqStudio is used for logging, an EV2300 or EV2400 PC interface board is required to interface to the gas gauge, and a PC USB cable is required for communication with a PC. Both can be ordered online at http://power.ti.com. Windows™-based PC software is available online as well. With the EV2300 or EV2400 interface board and software, the user can read the data registers, program the chipset for different configurations, log cycle data for further evaluation, and evaluate the overall functionality of the solution under different charge and discharge conditions.

This tool is an alternative to the existing Mathcad™ spreadsheet at https://www.ti.com/lit/zip/sluc042

This tool does not require the purchase of a separate Mathcad™ license.

Depending on the specific gas gauge product, bqStudio software may provide a packaging utility to create the zip file from the log files.

Note: This tool is not applicable to Compensated End of Discharge Voltage (CEDV) gauges.

Email gpc_support@list.ti.com for support issues related to use of this page.

TI's Standard Terms and Conditions for Evaluation Modules apply.

Battery fuel gauges
BQ20Z60-R1 SBS 1.1 compliant gas gauge with Impedance Track™ technology BQ27520-G4 System side Impedance Track™ fuel gauge with integrated LDO. BQ27532-G1 Battery management unit Impedance Track™ fuel gauge for bq2425x charger BQ27541-G1 Pack-side Impedance Track™ battery fuel gauge with integrated LDO BQ27542-G1 Single cell Impedance Track™ pack side fuel gauge with SON package BQ27545-G1 Single cell, pack side, Impedance Track™ fuel gauge BQ27546-G1 Single cell Impedance Track™ pack side fuel gauge with DSBGA package BQ27621-G1 System-side fuel gauge with Dynamic Voltage Correlation, battery gas gauge BQ27741-G1 Pack-side Impedance Track™(tm) fuel (gas) gauge with integrated protector BQ27742-G1 Single cell Li-ion battery fuel gauge with integrated protection | battery gas gauge BQ34Z100-G1 Multi-chemistry Impedance Track™ standalone fuel gauge | battery gas gauge BQ40Z50 1-4 series Li-ion battery pack manager | battery fuel (gas) gauge BQ40Z50-R1 1-4 series Li-ion battery pack manager supporting Turbo Mode 1.0 BQ40Z50-R2 1-4 series Li-ion battery pack manager supporting Turbo Mode 2.0 BQ40Z60 Complete multi-cell battery manager | battery fuel (gas) gauge

Get started

  1. Download the instruction manual for single or multiple cell (in series) battery pack and the data packaging tool (bqStudio) that creates zip file for upload
  2. Upload the zip file (login required)
  3. Gauging parameter calculation chemistry ID match report will be emailed to you, which will look like this sample report 

Technical documentation

No results found. Please clear your search and try again.
View all 1
Type Title Date
Application note Simple Guide to Chemical ID Selection Tool (GPC) (Rev. A) Jun. 05, 2018

Support & training

TI E2E™ forums with technical support from TI engineers

View all forum topics

Content is provided "as is" by TI and community contributors and does not constitute TI specifications. See terms of use.

If you have questions about quality, packaging or ordering TI products, see TI support.

Videos