Get started and develop with Bluetooth® low energy (BLE 5.x) solutions
Select a platform
LAUNCHXL-CC1352P1 — SimpleLink™ multiband CC1352P wireless MCU LaunchPad™ Development Kit, 2.4 GHz up to 5 dBm, 868/915 MHz pu to 20 dBm
LAUNCHXL-CC26X2R1 — SimpleLink™ CC26x2 Wireless MCU LaunchPad™ development kit
LP-CC2652RB — SimpleLink™ crystal-less BAW CC2652RB multiprotocol 2.4GHz wireless MCU LaunchPad™ development kit
LPSTK-CC1352R — SimpleLink™ multi band CC1352R wireless MCU LaunchPad™ SensorTag kit
SIMPLELINK-CC13XX-CC26XX-SDK — SimpleLink™ CC13xx and CC26xx software development kit (SDK)
Supported products & hardware
Products
Bluetooth products
Sub-1 GHz products
Wi-SUN products
Multi-protocol products
Hardware development
Evaluation board
SIMPLELINK-CC13XX-CC26XX-SDK — SimpleLink™ CC13xx and CC26xx software development kit (SDK)
Products
Bluetooth products
Sub-1 GHz products
Wi-SUN products
Multi-protocol products
Hardware development
Evaluation board
Documentation
Release Infomation
The SimpleLink™ CC13xx and CC26xx Software Development Kit (SDK) delivers components that enable engineers to develop applications on the Texas Instruments SimpleLink CC13xx and CC26xx family of wireless microcontrollers (MCUs). This software toolkit provides a cohesive and consistent software experience for all SimpleLink CC13xx and CC26xx wireless MCU users by packaging essential software components, such as a Bluetooth® Low Energy (BLE) protocol stack supporting Bluetooth 5.2, Bluetooth Mesh, Thread 1.1.1 networking stack based on OpenThread, Zigbee 3.0 compliant protocol suite, RF-Proprietary examples, TI’s 15.4 Stack as well as the TI-RTOS kernel and TI Drivers in one easy-to-use software package along with example applications and documentation. In addition, the Dynamic Multi-Protocol Manager (DMM) software component enables multiprotocol development on a single SimpleLink wireless MCU through time-division multiplexing.
The SimpleLink MCU portfolio offers a single development environment that delivers flexible hardware, software, and tool options for customers developing wired and wireless applications. With 100 percent code reuse across host MCUs, Wi-Fi™, Bluetooth Low Energy, Sub-1GHz devices and more, choose the MCU or connectivity standard that fits your design. A one-time investment with the SimpleLink software development kit allows you to reuse often, opening the door to create unlimited applications. For more information, visit www.ti.com/simplelink.
This is version 6.10.00.29 of the SimpleLink CC13xx/CC26xx SDK. For SimpleLink CC13x2 / CC26x2 SDK versions 5.20 and earlier, please see the SimpleLink CC13x2 / CC26x2 SDK download page
What's new
- New Proprietary RF example (rfDiagnostics) lets you use AT commands for RF testing
- Added ARIB support for TI 15.4 stack
- Added support for CC2651RSIPA
UNIFLASH — UniFlash for most TI microcontrollers (MCUs) and mmWave sensors
Supported products & hardware
Products
Automotive mmWave radar sensors
Arm-based microcontrollers
Bluetooth products
MSP430 microcontrollers
Sub-1 GHz products
C2000 real-time microcontrollers
Wi-Fi products
Wi-SUN products
Arm-based processors
Multi-protocol products
Industrial mmWave radar sensors
UNIFLASH — UniFlash for most TI microcontrollers (MCUs) and mmWave sensors
Products
Automotive mmWave radar sensors
Arm-based microcontrollers
Bluetooth products
MSP430 microcontrollers
Sub-1 GHz products
C2000 real-time microcontrollers
Wi-Fi products
Wi-SUN products
Arm-based processors
Multi-protocol products
Industrial mmWave radar sensors
Documentation
Release Infomation
UniFlash is a standalone tool used to program on-chip flash memory on TI MCUs and on-board flash memory for Sitara processors. UniFlash has a GUI, command line, and scripting interface. UniFlash is available free of charge.
What's new
- Device Support Update
- Device Support synced up with CCS11.2.0
- TMS320F280013x Flash Programming Support
- AWR29xx Flash Programming Support
- Bug Fixes
SENSOR-CONTROLLER-STUDIO — Sensor Controller Studio
Supported products & hardware
Products
Bluetooth products
Sub-1 GHz products
Wi-SUN products
Zigbee products
Multi-protocol products
Other wireless technologies
Hardware development
Development kit
SENSOR-CONTROLLER-STUDIO — Sensor Controller Studio
Installer executable
Compressed archive
Products
Bluetooth products
Sub-1 GHz products
Wi-SUN products
Zigbee products
Multi-protocol products
Other wireless technologies
Hardware development
Development kit
Documentation
Compressed source file archive
Release Infomation
Sensor Controller Studio is used to write, test and debug code for the CC26xx/CC13xx Sensor Controller, allowing for ultra-low power application design.
The tool generates a Sensor Controller Interface driver, which is a set of C source files to be compiled into the System CPU (ARM Cortex-M3/M4) application. These source files contain the Sensor Controller firmware image and associated definitions, and generic functions that allow the System CPU application to control the Sensor Controller and exchange data.
The Sensor Controller is a small CPU core that is highly optimized for low power consumption and efficient peripheral operation. The Sensor Controller is located in the CC26xx/CC13xx auxiliary (AUX) power/clock domain, and can perform simple background tasks autonomously and independently of the System CPU and the MCU domain power state. Such tasks include but are not limited to:
- Analog sensor polling, using ADC or comparator
- Digital sensor polling, using SPI, I2C or other protocols
- Capacitive sensing, using current source, comparator and time-to-digital converter (TDC)
- Waveform generation, for example for LCDs
The Sensor Controller is user programmable, using a simple programming language with syntax similar to C. This allows for sensor polling and other tasks to be specified as sequential algorithms, rather than static configuration of complex peripheral modules, timers, DMA, register programmable state machines, event routing and so on. The main advantages are:
- Flexibility
- Dynamic reuse of hardware resources
- Ability to perform simple data processing without need for dedicated hardware
- Observability and debugging options
What's new
- Added support for new devices: CC2672R3, CC2672P3, CC2662R-Q1, CC2652PSIP and CC2652P7.
- Added example support for new SDKs, using TI-RTOS 7 and GPIO driver for the latest CC13x2/CC26x2 SDK.
- Minor improvements.
- Bug-fixes.
SMARTRFTM-STUDIO — SmartRF Studio
Supported products & hardware
Products
Bluetooth products
MSP430 microcontrollers
Sub-1 GHz products
Wi-SUN products
Thread products
Zigbee products
Multi-protocol products
Other wireless technologies
Hardware development
Development kit
SMARTRFTM-STUDIO — SmartRF Studio
Products
Bluetooth products
MSP430 microcontrollers
Sub-1 GHz products
Wi-SUN products
Thread products
Zigbee products
Multi-protocol products
Other wireless technologies
Hardware development
Development kit
Documentation
Release Infomation
SmartRF™ Studio is a Windows application that can be used to evaluate and configure Low Power RF devices from Texas Instruments. The application helps designers of RF systems to easily evaluate the radio at an early stage in the design process. It is especially useful for generation of configuration register values and commands, and for practical testing and debugging of the RF system. SmartRF Studio can be used either as a standalone application or together with applicable evaluation boards or debug probes for the RF device.
What's new
- Added support for new devices: CC2653P10, CC2662R-Q1, CC2642R-Q1 and CC2651RSIPA
- New RF PHY settings for the CC1354x10 devices
- Updated TX Output power values for the CC13x4, CC26x4 and the CC2652PSIP devices
- Various improvements and bug-fixes
CCSTUDIO — Code Composer Studio™ integrated development environment (IDE)
Supported products & hardware
This design resource supports most products in these categories.
Check the product details page to verify support.
-
parametric-filter MSP430 microcontrollers -
parametric-filter C2000 real-time microcontrollers -
parametric-filter Arm-based microcontrollers -
parametric-filter Digital signal processors (DSPs) -
parametric-filter Arm-based processors -
parametric-filter Signal conditioners -
parametric-filter mmWave radar sensors -
parametric-filter Zigbee products -
parametric-filter Wi-Fi products -
parametric-filter Thread products -
parametric-filter Other wireless technologies -
parametric-filter Sub-1 GHz products -
parametric-filter Multi-protocol products -
parametric-filter Bluetooth products -
parametric-filter Digital power isolated controllers
Products
Automotive mmWave radar sensors
Industrial mmWave radar sensors
CCSTUDIO — Code Composer Studio™ integrated development environment (IDE)
Link to Windows single file (offline) installer for Code Composer Studio IDE (all features, devices)
Link to Linux single file (offline) installer for Code Composer Studio IDE (all features, devices)
Link to macOS single file (offline) installer for Code Composer Studio IDE (all features, devices)
Link to Windows on-demand (web) installer for Code Composer Studio IDE (all features, devices)
Link to Linux on-demand (web) installer for Code Composer Studio IDE (all features, devices)
Link to macOS on-demand (web) installer for Code Composer Studio IDE (all features, devices)
This design resource supports most products in these categories.
Check the product details page to verify support.
-
parametric-filter MSP430 microcontrollers -
parametric-filter C2000 real-time microcontrollers -
parametric-filter Arm-based microcontrollers -
parametric-filter Digital signal processors (DSPs) -
parametric-filter Arm-based processors -
parametric-filter Signal conditioners -
parametric-filter mmWave radar sensors -
parametric-filter Zigbee products -
parametric-filter Wi-Fi products -
parametric-filter Thread products -
parametric-filter Other wireless technologies -
parametric-filter Sub-1 GHz products -
parametric-filter Multi-protocol products -
parametric-filter Bluetooth products -
parametric-filter Digital power isolated controllers
Products
Automotive mmWave radar sensors
Industrial mmWave radar sensors
Documentation
Feature Overviews, App Notes and How-to Articles
Complete User's Guide
Release Infomation
The Code Composer Studio™ IDE is a complete integrated suite that enables developers to create and debug applications of all Texas Instruments Embedded Processors (Sitara, DSP, Automotive, Keystone), Microcontrollers (SimpleLink™, C2000 Digital Control, MSP430, TM4C, Hercules), as well as Digital Power (UCD) and Programmable Gain Amplifier (PGA) devices.
- Installation instructions
- System Requirements
- Update Status: This release will not be available as an update.
- Windows 32bit is not supported with CCSv11. If you are using a 32bit Windows System please use CCSv8.3.1.x or earlier.
- XDS510 class debug probes are not supported with CCSv11. Support for XDS510 class probes was deprecated years ago for Linux and macOS. If you need to use one of these older probes please use CCSv8.3.1 or earlier.
What's new
- Please refer to the release notes