Select a version
SIMPLELINK-SDK-WIFI-PLUGIN
SimpleLink™ software development kit (SDK) Wi-Fi® plug-in
Windows Installer for SimpleLink SDK Wi-Fi Plugin
macOS Installer for SimpleLink SDK Wi-Fi Plugin
Linux Installer for SimpleLink SDK Wi-Fi Plugin
Link to Windows Installer for SimpleLink CC3x20 Service Pack
Link to Mac Installer for SimpleLink CC3x20 Service Pack
Link to Linux Installer for SimpleLink CC3x20 Service Pack
Products
Wi-Fi products
Arm Cortex-M4 MCUs
Low-power 2.4-GHz products
Hardware development
Documentation
SimpleLink SDK Wi-Fi Plugin Users Guide
Wi-Fi Starter Pro mobile application for iOS and Android
Release Information
The SimpleLink™ SDK Wi-Fi Plugin is a companion software package that enables the use of a Wi-Fi radio on any standard MSP432 platform including the MSP432P401, MSP432P4111, and MSP432E401 families, as well as on the CC26X2R family of devices. By having the ability to seamlessly and modularly add Wi-Fi functionality to an embedded system, a programmer can enable their embedded device to become a gateway to various IOT infrastructures.
What's new
SimpleLink SDK 3.10.00.04
- Updated and validated against v2.40.00.xx of the MSP432P4/MSP432E4/CC26X2R1/CC32XX SDKs
SimpleLink CC3x20 Service Pack 3.11.1.0-2.0.0.0-2.2.0.6 - Released June 3rd, 2019
- Fixed critical CC3220/CC3120 NWP Issue which resulted in error and halt of execution, where the error state was persistent across device reset. This issue required a use case where the fast connect feature is enabled on the affected devices, and the AP that the device is connected to has at least two of the following authentication modes enabled: WPA2/PSK, WPA2/EAP, WPA2/FT using PSK (802.11r fast transition/fast roaming)