Texas Instruments makes designing with TMS320C5000™ DSPs easier with new credit-card-sized development tools
Low-cost eZdsp™ development tools plug directly into laptops via USB, allowing developers to create low power applications using TI’s C5502 and C5509A DSPs
Bangalore (April 14, 2011) — Today, Texas Instruments Incorporated (TI) announced the availability of new credit-card sized, low-cost TMDX5502EZDSP and TMDX5509EZDSP development tools, making TMS320C5000™ digital signal processor (DSP ) development easy and accessible for developers, hobbyists, researchers and students. The eZdsp™ development tools for C5502 and C5509A DSPs do not require any cables, allowing developers to simply plug the tool into the USB port of a laptop or workstation for hassle-free development and a simple out-of-the-box experience.
The eZdsp development tools feature up to 300 MHz of performance for the C5502 and 200 MHz for the C5509A. Containing a broad mix of interfacing options, these feature-packed eZdsp USB development tools are ideal for applications such as voice, audio, musical instruments and accessories, medical monitoring and fingerprint biometrics. To support rapid and easy development, both tools include a comprehensive suite of support software and sample code examples.
C5502 and C5509A eZdsp USB development tools key features and benefits
Feature |
Benefit |
Energy-efficient C5502 and C5509A DSPs featuring C5509A at 0.96mW/MHz at 200 MHz and 1.6V core and the C5502 at 1mW/MHz at 300 MHz and 1.26V core |
|
Integrated XDS100v2 emulator ($70 to $500 value) |
Eliminates the need to purchase a separate JTAG emulator to start development, lowering the upfront cost for DSP evaluation and making the tool more compact |
Free, complete Code Composer Studio (CCS) integrated development environment (IDE) v4 software ($2,000 value), optimized DSP library, Image Library, Telecom Library (fax and voice), Chip Support Library and on-board audio codecs and connectors |
Reduces development costs and allows quick and easy evaluation and development on the C5502 and C5509A DSPs for audio, voice, medical and other portable applications for faster time-to-market |
microSD card slot (on the C5509A eZdsp USB development tool), 512 kB SPI flash and 1 MB SDRAM |
Offers large data storage options and an option to store user program to SPI flash and boot from it to on-chip memory or SDRAM |
USB 1.1 slave (on the C5509A eZdsp USB development tool), Ethernet, Bluetooth and ZigBee connectors |
Enables evaluation of a range of connectivity options for developer’s applications |
Fingerprint biometric swipe sensor connector and extension connector |
Allows quick development of fingerprint access control system and the ability to design add-on cards for access to other serial ports on the DSP |
2.5’’ x 4’’ USB-powered form factor |
Improves user experience by having a simple and uncomplicated development platform |
Find out more about TI’s extensive C55x DSP portfolio by visiting:
About Texas Instruments
Texas Instruments (NYSE: TXN) helps customers solve problems and develop new electronics that make the world smarter, healthier, safer, greener and more fun. A global semiconductor company, TI innovates through design, sales and manufacturing operations in more than 30 countries. For more information, go to www.ti.com.
Trademarks
C5000, E2E and Code Composer Studio are trademarks of Texas Instruments. All other trademarks and registered trademarks belong to their respective owners.
India Product Information Centre
Toll: +91-80-4138 1665
Toll free: +1-800-425-7888
Email: tiasia@ti.com |