SBASAD2 November 2021 ADS130B04-Q1
PRODUCTION DATA
In a typical BMS, the current through
the shunt resistor must be measured in both directions for charging and discharging
the battery pack. In an overcurrent or short-circuit condition, the current can be
as high as IBAT_MAX = ±5 kA in this example application. Therefore, the
maximum voltage drop across the shunt is up to VSHUNT =
RSHUNT × IBAT_MAX = 35
μΩ × ±4 kA = ±140 mV.
In order to measure this shunt voltage, channel 2 of the ADS130B04-Q1 is configured for gain = 8, which allows differential voltage measurements of VIN2 = VAIN2P – VAIN2N = ±VREF / 8 = ±1.2 V / 8 = ±150 mV. The integrated charge pump in the device allows voltage measurements 300 mV below AGND for gains of 4 and higher while using a unipolar analog power supply. This bipolar voltage measurement capability is important because one side of the shunt is connected to the same GND potential as the AGND pin of the ADS130B04-Q1, which means that the absolute voltage that the device must measure is up to 140 mV below AGND.
To enable fast overcurrent detection within 1 ms while providing high accuracy and resolution, the ADS130B04-Q1 is operated at 4 kSPS (OSR = 1024, high-resolution mode) using global-chop mode. Global-chop mode enables measurements with minimal offset error over temperature and time. The conversion time using these settings is 0.754 ms according to Equation 6.
Channel 2 is selected for the shunt measurement on purpose because this channel generally shows the best offset error and offset drift with global-chop mode enabled across all four ADC channels. Of all the measurements, the offset performance is the most critical for the shunt measurement in a typical BMS.