SBAS562B April 2012 – December 2019 AMC1100
PRODUCTION DATA.
Current measurement through the phase of a motor power line is done via the shunt resistor RSHUNT (in a two-terminal shunt); see Figure 36. For better performance, the differential signal is filtered using RC filters (components R2, R3, and C2). Optionally, C3 and C4 can be used to reduce charge dumping from the inputs. In this case, care must be taken when choosing the quality of these capacitors; mismatch in values of these capacitors leads to a common-mode error at the modulator input. Using NP0 capacitors is recommended, if necessary.
The isolated voltage measurement can be performed as described in the Device Functional Modes section.