SLUSCD0B August 2015 – November 2018
PRODUCTION DATA.
Although the SMBus slave address is a configurable value in the bq78350-R1 device, this feature is disabled by default and the slave address is 0x16. The SMBus Address feature can allow up to nine different addresses based on external resistor value variation per address.
The default setup of the bq78350-R1 device is generic, but there are many additional features that can be enabled and configured to support a variety of system requirements. These are detailed in the bq78350-R1 Technical Reference Manual(SLUUBD3).