DLPS054H December 2015 – March 2024 DLPC230-Q1 , DLPC231-Q1
PRODUCTION DATA
The DLPC23x-Q1 provides 32 general purpose I/O that are available to support a variety of functions for a number of different product configurations. In general, most of these I/O will only support one specific function based on a specific product configuration, although that function can be different for a different product configuration. There are also a few of these I/O that have been reserved for use by the Host for whatever function they can require. In addition, most of these I/O can also be made available for TI test and debug use. Definitions for the HUD and Headlight product configurations are shown in Table 7-7 and Table 7-8.
GPIO | SIGNAL NAME | DESCRIPTION (1) |
---|---|---|
GPIO_00 | PMIC_CNTRL_OUT (input) | LED control feedback from the TPS99000-Q1. An external pulldown resistor must be used (connects to TPS99000-Q1 Drive Enable). |
GPIO_01 | PMIC_SEQ_STRT (output) | Sequence start output from the DLPC23x-Q1. This must be connected to the TPS99000-Q1 to time LED related actions and shadow TPS99000-Q1 configuration registers. An external pulldown resistor must be used. |
GPIO_02 | PMIC_COMP_OUT (input) | LED optical comparison feedback. This is used to count light pulses during each frame. This signal is active-low. An external pulldown resistor must be used. |
GPIO_03 | PMIC_LED_SEN (output) | LED Shunt Enable - shunts current from LEDs to allow faster LED turn-off. An external pulldown resistor must be used. |
GPIO_04 | PMIC_LED_DEN (output) | LED FET Drive Enable - enables LED current switching and defines LED pulse length. An external pulldown resistor must be used. |
GPIO_05 | Reserved for Future Use | An external pulldown resistor must be used |
GPIO_06 | Host Available | Available for general host use through host commands |
GPIO_07 | Host Available | Available for general host use through host commands |
GPIO_08 | Host Available | Available for general host use through host commands |
GPIO_09 | Reserved for Future Use | An external pulldown resistor must be used |
GPIO_10 | Reserved for Future Use | An external pulldown resistor must be used |
GPIO_11 | Reserved for Future Use | An external pulldown resistor must be used |
GPIO_12 | Reserved for Future Use | An external pulldown resistor must be used |
GPIO_13 | Reserved for Future Use | An external pulldown resistor must be used |
GPIO_14 | Reserved for Future Use | An external pulldown resistor must be used |
GPIO_15 | PMIC_WD1 (output) | Periodic signal that the DLPC23x-Q1 processor generates during normal operation. TPS99000-Q1 monitors this signal and reports if this signal stops pulsing. An external pulldown resistor must be used. |
GPIO_16 | Reserved for Future Use | An external pulldown resistor must be used |
GPIO_17 | Host Available | Available for general host use through host commands |
GPIO_18 | Reserved for Future Use | An external pulldown resistor must be used |
GPIO_19 | Reserved for Future Use | An external pulldown resistor must be used |
GPIO_20 | Reserved for Future Use | An external pulldown resistor must be used |
GPIO_21 | Reserved for Future Use | An external pulldown resistor must be used |
GPIO_22 | Reserved for Future Use | An external pulldown resistor must be used |
GPIO_23 | Reserved for Future Use | An external pulldown resistor must be used |
GPIO_24 | Reserved for Future Use | An external pulldown resistor must be used |
GPIO_25 | Reserved for Future Use | An external pulldown resistor must be used |
GPIO_26 | Host Available | Available for general host use through host commands |
GPIO_27 | Host Available | Available for general host use through host commands |
GPIO_28 | Host Available | Available for general host use through host commands |
GPIO_29 | Host Available | Available for general host use through host commands |
GPIO_30 | Host Available | Available for general host use through host commands |
GPIO_31 | Host Available | Available for general host use through host commands |
GPIO | SIGNAL NAME | DESCRIPTION (1) |
---|---|---|
GPIO_00 | HL_PWM0 (output) | PWM 0 Output - This can be used for general purposes such as controlling the level of an external light source. |
GPIO_01 | PMIC_SEQ_STRT (output) | Sequence start output from the DLPC23x-Q1. This must be connected to the TPS99000-Q1 to time LED related actions and shadow TPS99000-Q1 configuration registers. An external pulldown resistor must be used. |
GPIO_02 | HL_PWM1(output) | PWM 1 Output - This can be used for general purposes such as controlling the level of an external light source. |
GPIO_03 | Reserved for Future Use | An external pulldown resistor must be used |
GPIO_04 | Reserved for Future Use | An external pulldown resistor must be used |
GPIO_05 | Reserved for Future Use | An external pulldown resistor must be used |
GPIO_06 | Host Available | Available for general host use through host commands |
GPIO_07 | Host Available | Available for general host use through host commands |
GPIO_08 | Host Available | Available for general host use through host commands |
GPIO_09 | Reserved for Future Use | An external pulldown resistor must be used |
GPIO_10 | Reserved for Future Use | An external pulldown resistor must be used |
GPIO_11 | Reserved for Future Use | An external pulldown resistor must be used |
GPIO_12 | Reserved for Future Use | An external pulldown resistor must be used |
GPIO_13 | Reserved for Future Use | An external pulldown resistor must be used |
GPIO_14 | Reserved for Future Use | An external pulldown resistor must be used |
GPIO_15 | PMIC_WD1 (output) | Periodic signal that the DLPC23x-Q1 processor generates during normal operation. TPS99000-Q1 monitors this signal and reports if this signal stops pulsing. An external pulldown resistor must be used. |
GPIO_16 | Reserved for Future Use | An external pulldown resistor must be used |
GPIO_17 | HL_PWM2 (output) | PWM 2 Output - This can be used for general purposes such as controlling the level of an external light source. |
GPIO_18 | EXT_SMPL | Connects to TPS99000-Q1 EXT_SMPL input. This sequence-aligned signal can be configured to trigger TPS99000-Q1 ADC sampling. |
GPIO_19 | Reserved for Future Use | An external pulldown resistor must be used |
GPIO_20 | Reserved for Future Use | An external pulldown resistor must be used |
GPIO_21 | Reserved for Future Use | An external pulldown resistor must be used |
GPIO_22 | Reserved for Future Use | An external pulldown resistor must be used |
GPIO_23 | Reserved for Future Use | An external pulldown resistor must be used |
GPIO_24 | Reserved for Future Use | An external pulldown resistor must be used |
GPIO_25 | Reserved for Future Use | An external pulldown resistor must be used |
GPIO_26 | Host Available | Available for general host use through host commands |
GPIO_27 | Host Available | Available for general host use through host commands |
GPIO_28 | Host Available | Available for general host use through host commands |
GPIO_29 | Host Available | Available for general host use through host commands |
GPIO_30 | Host Available | Available for general host use through host commands |
GPIO_31 | Host Available | Available for general host use through host commands |