SLLSEC6E September 2012 – June 2019 DP83848-EP
PRODUCTION DATA.
The DP83848-EP pins are classified into the following interface categories (each interface is described in the sections that follow):
All DP83848-EP signal pins are I/O cells regardless of the particular use. The definitions below define the functionality of the I/O cells for each pin.
NOTE
Strapping pin option. See Table 3-8 for strap definitions.