7 |
GPIO2_OUTPUT
_VALUE
_D_GPOI2_OUTPUT
_VALUE |
R/W |
0h |
GPIO1/GPIO2 and D_GPIO1/D_GPIO2 Configuration
If PORT1_SEL is set, this register controls the D_GPIO1 and D_GPIO2 pins
Local GPIO Output Value
This value is output on the GPIO pin when the GPIO function is enabled, the local GPIO direction is Output, and remote GPIO control is disabled. |
6 |
GPIO2_REMOTE
_ENABLE
_D_GPIO2_REMOTE
_ENABLE |
R/W |
0h |
Remote GPIO Control
1: Enable GPIO control from remote Serializer. The GPIO pin will be an output, and the value is received from the remote Serializer.
0: Disable GPIO control from remote Serializer. |
5 |
GPIO2_DIR
_D_GPIO2_DIR |
R/W |
0h |
The GPIO DIR configures the pad in input direction or output direction for functional mode or GPIO mode.
00: Functional mode; output
10: Tri-state
01: GPIO mode; output
11: GPIO mode; input |
4 |
GPIO2_EN
_D_GPIO2_EN |
R/W |
0h |
The GPIO EN configures the pad in input direction or output direction for functional mode or GPIO mode.
00: Functional mode; output
10: Tri-state
01: GPIO mode; output
11: GPIO mode; input |
3 |
GPIO1_OUTPUT
_VALUE
_D_GPIO1_OUTPUT
_VALUE |
R/W |
0h |
Local GPIO Output Value
This value is output on the GPIO pin when the GPIO function is enabled, the local GPIO direction is Output, and remote GPIO control is disabled. |
2 |
GPIO1_REMOTE
_ENABLE
_D_GPIO1_REMOTE
_ENABLE |
R/W |
0h |
Remote GPIO Control
1: Enable GPIO control from remote Serializer. The GPIO pin will be an output, and the value is received from the remote Serializer.
0: Disable GPIO control from remote Serializer. |
1 |
GPIO1_DIR
_D_GPIO1_DIR |
R/W |
0h |
The GPIO DIR configures the pad in input direction or output direction for functional mode or GPIO mode.
00: Functional mode; output
10: Tri-state
01: GPIO mode; output
11: GPIO mode; input |
0 |
GPIO1_EN
_D_GPIO1_EN |
R/W |
0h |
The GPIO EN configures the pad in input direction or output direction for functional mode or GPIO mode.
00: Functional mode; output
10: Tri-state
01: GPIO mode; output
11: GPIO mode; input |