SNAS689A October 2017 – July 2019 LMK04228
PRODUCTION DATA.
The following section details the fields of each register, the poweron-reset (POR) defaults, and specific descriptions of each bit.
In some cases similar fields are located in multiple registers. In this case specific outputs may be designated as X or Y. In these cases the X will represent even numbers from 0 to 12 and the Y will represent odd numbers from 1 to 13. In the case where X and Y are both used in a bit name, then Y = X + 1.