SLLSF04D April 2018 – June 2022 TLIN1024-Q1
PRODUCTION DATA
When using the TLIN1024-Q1 in systems which are monitoring the RXD pin for a wake up request, special care should be taken during the mode transitions. The output of the RXD pin is indeterminate for the transition period between states as the receivers are switched. The application software should not look for an edge on the RXD pin indicating a wake up request until tMODE_CHANGE plus tNOMINT when going from sleep or standby to normal mode. This is shown in Figure 7-15