SPRS797C November 2012 – October 2018 TMS320F28050 , TMS320F28051 , TMS320F28052 , TMS320F28053 , TMS320F28054 , TMS320F28055
PRODUCTION DATA.
Figure 6-12 shows how the various interrupt sources are multiplexed.
Eight PIE block interrupts are grouped into one CPU interrupt. In total, 12 CPU interrupt groups, with 8 interrupts per group equals 96 possible interrupts. Table 6-23 shows the interrupts used by 2805x devices.
The TRAP #VectorNumber instruction transfers program control to the interrupt service routine (ISR) corresponding to the vector specified. TRAP #0 attempts to transfer program control to the address pointed to by the reset vector. The PIE vector table does not, however, include a reset vector. Therefore, TRAP #0 should not be used when the PIE is enabled. Doing so will result in undefined behavior.
When the PIE is enabled, TRAP #1 to TRAP #12 will transfer program control to the ISR corresponding to the first vector within the PIE group. For example: TRAP #1 fetches the vector from INT1.1, TRAP #2 fetches the vector from INT2.1, and so forth.
INTx.8 | INTx.7 | INTx.6 | INTx.5 | INTx.4 | INTx.3 | INTx.2 | INTx.1 | |
---|---|---|---|---|---|---|---|---|
INT1.y | WAKEINT | TINT0 | ADCINT9 | XINT2 | XINT1 | Reserved | ADCINT2 | ADCINT1 |
(LPM/WD) | (TIMER 0) | (ADC) | Ext. int. 2 | Ext. int. 1 | – | (ADC) | (ADC) | |
0xD4E | 0xD4C | 0xD4A | 0xD48 | 0xD46 | 0xD44 | 0xD42 | 0xD40 | |
INT2.y | Reserved | EPWM7_TZINT | EPWM6_TZINT | EPWM5_TZINT | EPWM4_TZINT | EPWM3_TZINT | EPWM2_TZINT | EPWM1_TZINT |
– | (ePWM7) | (ePWM6) | (ePWM5) | (ePWM4) | (ePWM3) | (ePWM2) | (ePWM1) | |
0xD5E | 0xD5C | 0xD5A | 0xD58 | 0xD56 | 0xD54 | 0xD52 | 0xD50 | |
INT3.y | Reserved | EPWM7_INT | EPWM6_INT | EPWM5_INT | EPWM4_INT | EPWM3_INT | EPWM2_INT | EPWM1_INT |
– | (ePWM7) | (ePWM6) | (ePWM5) | (ePWM4) | (ePWM3) | (ePWM2) | (ePWM1) | |
0xD6E | 0xD6C | 0xD6A | 0xD68 | 0xD66 | 0xD64 | 0xD62 | 0xD60 | |
INT4.y | Reserved | Reserved | Reserved | Reserved | Reserved | Reserved | Reserved | ECAP1_INT |
– | – | – | – | – | – | – | (eCAP1) | |
0xD7E | 0xD7C | 0xD7A | 0xD78 | 0xD76 | 0xD74 | 0xD72 | 0xD70 | |
INT5.y | Reserved | Reserved | Reserved | Reserved | Reserved | Reserved | Reserved | EQEP1_INT |
– | – | – | – | – | – | – | (eQEP1) | |
0xD8E | 0xD8C | 0xD8A | 0xD88 | 0xD86 | 0xD84 | 0xD82 | 0xD80 | |
INT6.y | Reserved | Reserved | Reserved | Reserved | Reserved | Reserved | SPITXINTA | SPIRXINTA |
– | – | – | – | – | – | (SPI-A) | (SPI-A) | |
0xD9E | 0xD9C | 0xD9A | 0xD98 | 0xD96 | 0xD94 | 0xD92 | 0xD90 | |
INT7.y | Reserved | Reserved | Reserved | Reserved | Reserved | Reserved | Reserved | Reserved |
– | – | – | – | – | – | – | – | |
0xDAE | 0xDAC | 0xDAA | 0xDA8 | 0xDA6 | 0xDA4 | 0xDA2 | 0xDA0 | |
INT8.y | Reserved | Reserved | SCITXINTC | SCIRXINTC | Reserved | Reserved | I2CINT2A | I2CINT1A |
– | – | (SCI-C) | (SCI-C) | – | – | (I2C-A) | (I2C-A) | |
0xDBE | 0xDBC | 0xDBA | 0xDB8 | 0xDB6 | 0xDB4 | 0xDB2 | 0xDB0 | |
INT9.y | Reserved | Reserved | ECAN1_INTA | ECAN0_INTA | SCITXINTB | SCIRXINTB | SCITXINTA | SCIRXINTA |
– | – | (CAN-A) | (CAN-A) | (SCI-B) | (SCI-B) | (SCI-A) | (SCI-A) | |
0xDCE | 0xDCC | 0xDCA | 0xDC8 | 0xDC6 | 0xDC4 | 0xDC2 | 0xDC0 | |
INT10.y | ADCINT8 | ADCINT7 | ADCINT6 | ADCINT5 | ADCINT4 | ADCINT3 | ADCINT2 | ADCINT1 |
(ADC) | (ADC) | (ADC) | (ADC) | (ADC) | (ADC) | (ADC) | (ADC) | |
(ePWM16) | (ePWM15) | (ePWM14) | (ePWM13) | (ePWM12) | (ePWM11) | (ePWM10) | (ePWM9) | |
0xDDE | 0xDDC | 0xDDA | 0xDD8 | 0xDD6 | 0xDD4 | 0xDD2 | 0xDD0 | |
INT11.y | CLA1_INT8 | CLA1_INT7 | CLA1_INT6 | CLA1_INT5 | CLA1_INT4 | CLA1_INT3 | CLA1_INT2 | CLA1_INT1 |
(CLA) | (CLA) | (CLA) | (CLA) | (CLA) | (CLA) | (CLA) | (CLA) | |
(ePWM16) | (ePWM15) | (ePWM14) | (ePWM13) | (ePWM12) | (ePWM11) | (ePWM10) | (ePWM9) | |
0xDEE | 0xDEC | 0xDEA | 0xDE8 | 0xDE6 | 0xDE4 | 0xDE2 | 0xDE0 | |
INT12.y | LUF | LVF | Reserved | Reserved | Reserved | Reserved | Reserved | XINT3 |
(CLA) | (CLA) | – | – | – | – | – | Ext. Int. 3 | |
0xDFE | 0xDFC | 0xDFA | 0xDF8 | 0xDF6 | 0xDF4 | 0xDF2 | 0xDF0 |
NAME | ADDRESS | SIZE (×16) | DESCRIPTION(1) |
---|---|---|---|
PIECTRL | 0x0CE0 | 1 | PIE, Control register |
PIEACK | 0x0CE1 | 1 | PIE, Acknowledge register |
PIEIER1 | 0x0CE2 | 1 | PIE, INT1 Group Enable register |
PIEIFR1 | 0x0CE3 | 1 | PIE, INT1 Group Flag register |
PIEIER2 | 0x0CE4 | 1 | PIE, INT2 Group Enable register |
PIEIFR2 | 0x0CE5 | 1 | PIE, INT2 Group Flag register |
PIEIER3 | 0x0CE6 | 1 | PIE, INT3 Group Enable register |
PIEIFR3 | 0x0CE7 | 1 | PIE, INT3 Group Flag register |
PIEIER4 | 0x0CE8 | 1 | PIE, INT4 Group Enable register |
PIEIFR4 | 0x0CE9 | 1 | PIE, INT4 Group Flag register |
PIEIER5 | 0x0CEA | 1 | PIE, INT5 Group Enable register |
PIEIFR5 | 0x0CEB | 1 | PIE, INT5 Group Flag register |
PIEIER6 | 0x0CEC | 1 | PIE, INT6 Group Enable register |
PIEIFR6 | 0x0CED | 1 | PIE, INT6 Group Flag register |
PIEIER7 | 0x0CEE | 1 | PIE, INT7 Group Enable register |
PIEIFR7 | 0x0CEF | 1 | PIE, INT7 Group Flag register |
PIEIER8 | 0x0CF0 | 1 | PIE, INT8 Group Enable register |
PIEIFR8 | 0x0CF1 | 1 | PIE, INT8 Group Flag register |
PIEIER9 | 0x0CF2 | 1 | PIE, INT9 Group Enable register |
PIEIFR9 | 0x0CF3 | 1 | PIE, INT9 Group Flag register |
PIEIER10 | 0x0CF4 | 1 | PIE, INT10 Group Enable register |
PIEIFR10 | 0x0CF5 | 1 | PIE, INT10 Group Flag register |
PIEIER11 | 0x0CF6 | 1 | PIE, INT11 Group Enable register |
PIEIFR11 | 0x0CF7 | 1 | PIE, INT11 Group Flag register |
PIEIER12 | 0x0CF8 | 1 | PIE, INT12 Group Enable register |
PIEIFR12 | 0x0CF9 | 1 | PIE, INT12 Group Flag register |
Reserved | 0x0CFA –
0x0CFF |
6 | Reserved |